这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家联系

16500B Operating System Software (Version 3.14)

These files contain the 3.14 OP SYS for the 16500B and are dated 07/18/97. (Note: These are DOS files. DO NOT use the lifutil to copy.)

All files on these 5 disks should be copied into the '\SYSTEM' directory on the 16500B hard disk drive.

The 3.14 version is the same as the 3.13 version except for the 'SYS_034' file which has been updated to support the E2474A. If you/customer already has version 3.13 installed...just 'get' the 'SYS_034' (on Disk #4) file and copy it over the existing 'SYS_034' file on the 16500B Hard Drive.

Version 3.14 or later of the 16500B operating system is required to work with the the E2474A.

发布日期 版本 版本说明
1997-08-04 3.14 Operating system software files for the 16500B logic analysis system.

如何下载

  • Click the download button, select file and save.

如何安装

  • See Documentation

颁发许可证

  • 不要求具有许可证