Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

IO Libraries Suite Downloads

To find out more about the IO Libraries Suite, visit www.keysight.com/find/iosuite

IO Libraries Suite 2018 adds support for the following features:

  • E8491B FireWire to VXI on Windows 10

A number of defects were fixed, including:

  • Issues that caused crashes in:
    • Connection Expert (44266, 44271, 44274)
    • Various I/O services and tools when "FIPS compliant algorithms” was enabled (44410)
    • Interactive IO if too much data was transferred (46070)
    • PXI Resource Manager if defective PXI drivers were encountered (45871)
  • Some issues where the Discovery Service and Connection Expert would become unresponsive (44459)
  • Issue where IO Monitor might display different timestamps if a log is opened on different systems (41227)
  • A PXI issue where aliases were only returned if they were defined on the “Legacy” form of the PXI VISA address (44140)
  • Issue where updating the Active PXI Resource Manager could cause other vendors to lock the configuration.ini file incorrectly (41367)
  • Various other defects

The following enhancements were made to address defects:

  • The PXI Resource Manager now monitors for new devices for 5 minutes after boot (44265)
  • Added the ability to copy data out of IO Monitor to the clipboard (41272)
  • Added an option in IO Monitor to “Automatically Capture Messages on Startup” (44685)
     
Release Date Version Version Description
2017-10-11 2018 See description above. Build 18.1.22603.1.

How to Download

  • Click the download link and save the installer.

How to Install

  • Run the downloaded installer.

Licensing

  • Does Not Require a License

Supporting Documentation

Download

Installs on:

PC

Operating System

  • Windows 10
  • Windows 8.1
  • Windows 7 SP1
  • Windows Server 2012 (64-bit only)
  • Windows Server 2008 R2 SP1 (64-bit only)

Prerequisites

  • Information Not Available

Supported Instruments

  • All instruments.

Related Links