What are you looking for?
Suggested searches
No product matches found - System Exception
Matched content
N4010A Bluetooth® EDR Tx/Rx (DLL)
Installation Procedure
- Close all applications on the installation PC
- Insert the Intallation CD-ROM in the PC/DVD drive
Wait until the Install Wizard has completed and the Welcome window is displayed - Select "Next" on the Welcome screen to continue NOTE: It is required to have Microsoft® .NET framework verson 1.1 (or greater) already installed on your PC, see the Installation Guide for further details
- Review the terms of the licenses agreement, make the appropriate selection and select "Next" to continue
- Select "Next" to accept the default install path (recommended) or select "Change" and enter the new path
- Select "Next" to being the installation
- Select "Close" when the Install Wizard complete screen is displayed to close the installation
Bluetooth and the Bluetooth logos are trademarks owned by Bluetooth SIG, Inc., U.S.A. and licensed to Keysight Technologies, Inc.
Windows and MS Windows are U.S. registered trademarks of Microsoft Corporation.
Keysight recommends using the most current version, which includes the most up-to-date bug fixes and security patches available.
Release Date | Version | Version Description |
---|---|---|
2006-01-25 | n/a | Download this file and double click on it to install the DLL. |
Release Date | Version |
---|---|
2006-01-25 | n/a |
Version Description |
---|
Download this file and double click on it to install the DLL. |
How to Download
- Information Not Available
How to Install
See Above
Licensing
- Requires a License
Supporting Documentation
Installs on: PC / Instrument
Prerequisites
- Information Not Available
Supported Instruments
- N4010A
No previous versions available
SHOW MORE