What are you looking for?
Suggested searches
No product matches found - System Exception
Matched content
ART/AQT/Intelligent Test Framework Software Solution 3.0d
This patch includes fixes across three main applications, ART, AQT and ITF. The patch for ART and AQT are included inside one patch file and there are RepairTool30d and QualityTool10d respectively. This patch is accumulative in nature and contains all fixes released in the last release (ITF 3.0a patch).
Software patch revision 3.0d addresses these issues:
Description | Change Request Identification |
---|---|
ITF: Lifetime Rules can now delete Natives files and solid shape model images | CR14781 and CR15132 |
ITF: Fix for broken file caused by the network congestion between SJ and ITF | CR15103 |
ITF: Fix for broken file issues caused by network congestion | CR15291 |
ITF: Added Retry All and Delete All buttons on the Broken file view of the ITF Administration system | CR13903 |
ITF: Fixed data loss problem on multiple board panel when one board has 40 times more defects than others | CR15109 |
ART: Fixed missing images when using SJ ANDed algorithm (for SJ AOI), specifically those using RefDef suffix "-sh" | CR15190 |
ART: Fixed missing defect call on a primary component when using SJ ANDed algorithm with RefDef suffix "-sh" | CR15133 |
ART: SP50 defects can now be opened in ART | CR15289 |
ART: Search for Board by Type dialog box has time stamp on each board type or panel name inside the left pane | CR14978 |
ART: Fixed delay in data retrieval when opening Boards in sequence or Non-Barcode mode for AOI | CR15637 |
AQT: SP50 defect attributes can now be charted in AQT. Note that ITF and AQT on this patch are not handling measurement data | CR15290 |
Software patch revision 3.0d installation instructions:
- Download the patch, ITF Server 3.0d onto the ITF Server.
- On the ITF Server, make sure the ITF services are stopped.
Double-click on the file C:\Program Files\Keysight Technologies\Intelligent Test Framework\Util\Diag\Stop.bat. - Install the ITF Server patch components.
Double-click on ITFServer30d.exe self-extracting executable file.
Follow the instructions in the Install Shield.
If you have a 5DX connected to the ITF, you will need to modify your TRCMDPRO.CMD. For details of modification, please refer to the release notes. - If you have an ART Client, install the ART patch components on the Repair Clients. The extraction included the patches for ART. These files were extracted in the shared "C:\Program Files\Keysight Technologies\Intelligent Test Framework\Install\Repair" directory.
Go to the ART Client PC and map a drive to the ITF Server "Install" directory to download the ART patch.
While on the ART Client PC, double click on the file RepairTool30d.exe. This will install the patch for the ART Client. - If you have an AQT Client, install the AQT patch components on the Repair Clients. The extraction included the patches for AQT. These files were extracted in the shared "C:\Program Files\Keysight Technologies\Intelligent Test Framework\Install\Quality" directory.
Go to the AQT Client PC and map a drive to the ITF Server "Install" directory to download the ART patch.
While on the AQT Client PC, double click on the file QualityTool10d.exe. This will install the patch for the AQT Client. - If you have a Keysight SJ Series connected to ITF, install the new ITFSJComponents30d.exe. For details of applying this package, please refer to the release notes.
Keysight recommends using the most current version, which includes the most up-to-date bug fixes and security patches available.
Release Date | Version | Version Description |
---|---|---|
2004-08-02 | 3.0d | N/A |
Release Date | Version |
---|---|
2004-08-02 | 3.0d |
Version Description |
---|
N/A |
How to Download
- See Above
How to Install
- See Above
Licensing
- Does Not Require a License
Supporting Documentation
No previous versions available
SHOW MORE