What are you looking for?
3070 05.31 Board Conversion Tool for B.03.6x and B.03.8x Test Systems
The Keysight 3070 Board Conversion tool is used to convert the ASCII text files in a board directory for cross-platform compatibility between HP-UX and MS Windows operating systems. Text files contained in the board directory are merged into a single compressed file. The executable files are regenerated by IPG Test Consultant.
A version of the conversion tool is already installed on all Keysight 3070/79000 controllers with version 04.00 or later software. This download will install the Conversion tool onto HP-UX controllers with older B.03.6x or B.03.8x software.
The conversion tool will not work properly on a board directory that is corrupt, or one which has missing source files. Before converting a board directory you should run Test Consultant to check it's integrity.
3070 B.03.6x or B.03.8x software must be installed on your HP-UX system before installing Keysight 3070 Conversion Tool.
To download on Unix systems running 3070 B.03.6X or B.03.8X software releases:
- Click on "3070 Conversion Tool 05.31 UX Download." Approximately 4 MB of available space will be necessary to perform the decompression, and the final decompressed size of the file will be 2.2 MB.
- In the download box, change the "Selection:" to reflect the location to which you want to download (/var/tmp/cTool_05.31.pkg is recommended).
- Change to the directory to which the software package was downloaded (/var/tmp).
- Users already familiar with swinstall, may continue installation specifying a "Source Depot Type" of "Local Directory" and a "Source Depot Path..." of "/var/tmp/cTool_05.31.pkg". Users not familiar with swinstall should click on "Swinstall Instructions" to download detailed instructions. In a shell window, enter: "/usr/local/bin/X11/acroread [path/]UsingSwinstall.PDF".
- To download documentation on the Conversion tool, click on "Conversion Tool Instructions". To view this file, in a shell window enter: "/usr/local/bin/X11/acroread [path/]BoardConvert.PDF.
Release Date | Version | Version Description |
---|---|---|
2004-03-31 | 05.31 | 3070 Conversion Tool 05.31 UX Download |
Release Date | Version |
---|---|
2004-03-31 | 05.31 |
Version Description |
---|
3070 Conversion Tool 05.31 UX Download |
How to Download
- See Above
How to Install
Licensing
- Does Not Require a License