What are you looking for?
Keysight i1000D 03.51p Software Release
Keysight Technologies is pleased to introduce the 3.51p software release for existing i1000D series of in-circuit testers. This release can be installed on testheads and test development stations with Windows 7 (32-bit and 64-bit) operating system. Some of the highlights include:
− PVF Enhancement
− New “Abort” Function
− Enhanced I2C Feature
− Support 10KHz for TestJet
− Pins Test
− Shorts Learning Log File
− Transformer Mode
− Program Support Script
− Diagnostics GUI Ehancement
Veröffentlichungsdatum | Version | Versionsbeschreibung |
---|---|---|
2016-11-01 | 3.51p | Keysight i1000 Software Release Version 3.51p |
Veröffentlichungsdatum | Version |
---|---|
2016-11-01 | 3.51p |
Version Description |
---|
Keysight i1000 Software Release Version 3.51p |
How to Download
Click the "Download" button.
Save file to a folder in C: drive of PC.
How to Install
The installer will automatically prompt to install the i1000 software & the 3rd party software required.
1. Double click on the appropriate installer file.
2. Select “I accept the agreement” option and click Next.
3. The next screen shows a list of plug-in modules that will be installed. Click Next.
4. Select “Create a desktop icon”. Click Next.
5. Click Install to start the i1000 software installation.
6. USB Host driver will be installed automatically after the installation of the drivers.
7. Select “I accept the terms of the license agreement”. Click Next.
8. Click Install. This may take a few minutes. Click Finish when the installation is completed.
9. Java is required for the i1000 software to operate. Click Install.
10. After the Java installation is completed, it will proceed to install Microsoft® .NET Framework.
11. Click Finish to complete the installation. The i1000 software is now installed.
Lizenzierung
- Requires a License
Supporting Documentation
Installs on: PC
Operating System
- Windows 7
Voraussetzungen
No prerequisite required.
Supported Instruments
- U9401B Keysight i1000D Press Down ICT System, U9403A Keysight Mini ICT System, U9405A Keysight i1000D Small Foot Print ICT System (Inline/Offline)