This printer driver is only used for the 4287A with the following serial numbers and for operating the HP DeskJet 5550 with the 4287A. This driver is not required if the driver has already been installed into the 4287A.
4287A JP1KJ00101 through 754

Installation Procedure
Step1. Prepare one floppy disk.
Step2. Insert the floppy disk into your computer's FDD.
Step3. Click on the "Printer driver" listed below.
Step4. Copy the file onto the disk.
Step5. Click on the "Printer Driver (for HP DeskJet 5550) Installation" listed below,
and follow the installation manual.

Keysight recommends using the most current version, which includes the most up-to-date bug fixes and security patches available.
Release Date Version Version Description
2003-06-06 n/a Printer Driver
Release Date Version
2003-06-06 n/a
Version Description
Printer Driver

How to Download

  • See Above

How to Install

  • See Above

Licensing

  • Does Not Require a License

Installs on: Instrument

Operating System

  • Windows 95/98

Prerequisites

  • See Above

Supported Instruments

  • 4287A
No previous versions available
SHOW MORE