Keysight recommends using the most current version, which includes the most up-to-date bug fixes and security patches available.
Release Date Version Version Description
2015-12-09 01.00.0003 The N7015A/N7016A USB Type-C Interconnect Assembly Controller software is used to configure the hardware settings of the low speed fixture.
Release Date Version
2015-12-09 01.00.0003
Version Description
The N7015A/N7016A USB Type-C Interconnect Assembly Controller software is used to configure the hardware settings of the low speed fixture.

How to Download

  • Click the download button and save the file to a temporary directory on your Infiniium oscilloscope or personal computer.

How to Install

  • The N7015A/N7016A USB Type-C Interconnect Assembly Controller software should be installed on the Infiniium oscilloscope or personal computer that will be used to configure the hardware settings of the N7016A low speed fixture.

  • To install the software, open (execute) the downloaded file, and follow the on-screen installation instructions.

Licensing

  • Does Not Require a License

Installs on: PC / Instrument

Operating System

  • Windows 7
  • Windows Vista

Prerequisites

  • Microsoft .NET 4.5.2 software

Supported Instruments

  • N7016A Low Speed Fixture
No previous versions available
SHOW MORE