您希望搜索哪方面的内容?
建议的搜索
No product matches found - System Exception
符合的结果
N8900 系列自动量程系统直流电源固化软件
是德建议使用最新的版本,其中包括最新的漏洞修复和安全补丁
发布日期 | 版本 | 版本说明 |
---|---|---|
2022-01-21 | C.02.08.769 | N8900 series firmware version C.02.08.769 |
发布日期 | 版本 |
---|---|
2022-01-21 | C.02.08.769 |
版本说明 |
---|
N8900 series firmware version C.02.08.769 |
如何下载
- Click the Download button.
- Save the file to your computer and note the directory where the file is saved. A firmware update installed over the LAN, GPIB, or USB interface is a file with a .upd extension.
- Unzip the file to access the .upd file.
如何安装
- From the utility directory or Start menu, start the utility (FWUpdate.exe). The utility will prompt you for the location of the .upd file. Follow the additional prompts to complete the installation. The update may take several seconds to complete and will reboot the instrument. After the update is complete, exit the utility.
- It is not necessary to re-calibrate the instrument following a firmware-update; however, the instrument may need to be re-secured if it was unsecured to perform the update.
颁发许可证
- Does Not Require a License
支持文档
附加的软件/实用程序
Installs on: Instrument
操作系统
- Windows 7
- Windows XP
- Windows 2000
- Windows NT
- Windows ME
前提要求
- Information Not Available
支持的仪器
- N8920A, N8921A, N8923A, N8924A, N8925A, N8926A, N8928A, N8929A, N8930A, N8931A, N8932A, N8934A, N8935A, N8937A, N8940A, N8941A, N8943A, N8944A, N8945A, N8946A, N8948A, N8949A, N8950A, N8951A, N8952A, N8954A, N8955A, N8957A
如何下载
- Click the Download button.
- Save the file to your computer and note the directory where the file is saved. A firmware update installed over the LAN, GPIB, or USB interface is a file with a .upd extension.
- Unzip the file to access the .upd file.
如何安装
- From the utility directory or Start menu, start the utility (FWUpdate.exe). The utility will prompt you for the location of the .upd file. Follow the additional prompts to complete the installation. The update may take several seconds to complete and will reboot the instrument. After the update is complete, exit the utility.
- It is not necessary to re-calibrate the instrument following a firmware-update; however, the instrument may need to be re-secured if it was unsecured to perform the update.
颁发许可证
- 不要求具有许可证
支持文档
附加的软件/实用程序
安装到: Instrument
操作系统
- Windows 7
- Windows XP
- Windows 2000
- Windows NT
- Windows ME
前提要求
- 无此信息
支持的仪器
- N8920A, N8921A, N8923A, N8924A, N8925A, N8926A, N8928A, N8929A, N8930A, N8931A, N8932A, N8934A, N8935A, N8937A, N8940A, N8941A, N8943A, N8944A, N8945A, N8946A, N8948A, N8949A, N8950A, N8951A, N8952A, N8954A, N8955A, N8957A
如何下载
- Click the Download button.
- Save the file to your computer and note the directory where the file is saved. A firmware update installed over the LAN, GPIB, or USB interface is a file with a .upd extension.
- Unzip the file to access the .upd file.
如何安装
- From the utility directory or Start menu, start the utility (FWUpdate.exe). The utility will prompt you for the location of the .upd file. Follow the additional prompts to complete the installation. The update may take several seconds to complete and will reboot the instrument. After the update is complete, exit the utility.
- It is not necessary to re-calibrate the instrument following a firmware-update; however, the instrument may need to be re-secured if it was unsecured to perform the update.
颁发许可证
- 不要求具有许可证
支持文档
附加的软件/实用程序
安装到: Instrument
操作系统
- Windows 7
- Windows XP
- Windows 2000
- Windows NT
- Windows ME
前提要求
Download and install Firmware Update Utility software
支持的仪器
- N8920A, N8921A, N8923A, N8924A, N8925A, N8926A, N8928A, N8929A, N8930A, N8931A, N8932A, N8934A, N8935A, N8937A, N8940A, N8941A, N8943A, N8944A, N8945A, N8946A, N8948A, N8949A, N8950A, N8951A, N8952A, N8954A, N8955A, N8957A
如何下载
- 点击“下载”按钮。
- 将文件保存到您的计算机中,并指定目标文件夹。固化软件更新版本通过 LAN、GPIB 或 USB 接口进行安装,它是一个扩展名为 .upd 的文件。
- 解压并且访问这个 .upd 文件。
如何安装
在实用程序目录或“开始”菜单中,启动该实用程序(FWUpdate.exe)。它会提示您 .upd 文件的位置。根据进一步的提示完成安装。更新过程将持续数秒钟,并要求重启仪器。更新完毕后,退出该实用程序。
无需对固化软件更新后的仪器重新校准;但如果仪器在更新时解除了安全特性锁定,则需要重新锁定。
颁发许可证
- 不要求具有许可证
支持文档
附加的软件/实用程序
安装到: Instrument
操作系统
- Windows 7
- Windows XP
- Windows 2000
- Windows NT
- Windows ME
前提要求
- 无此信息
支持的仪器
- N8920A, N8921A, N8923A, N8924A, N8925A, N8926A, N8928A, N8929A, N8930A, N8931A, N8932A, N8934A, N8935A, N8937A, N8940A, N8941A, N8943A, N8944A, N8945A, N8946A, N8948A, N8949A, N8950A, N8951A, N8952A, N8954A, N8955A, N8957A
如何下载
- 点击下载按钮。
- 将文件保存到您的计算机中,并指定目标文件夹。固化软件更新版本是一个扩展名为 .upd 的文件,通过 LAN、GPIB 或 USB 接口安装。
-
解压并且访问这个 .upd 文件。
如何安装
在实用工具目录或开始菜单中,启动该实用工具(FWUpdate.exe)。它会提示您 .upd 文件的位置。根据额外的提示完成安装。更新过程将持续数秒钟,并要求重启仪器。更新完毕后,退出该实用工具。
固化软件更新后的仪器无需重新校准;但如果仪器在更新时解除了安全特性锁定,则需要重新锁定。
颁发许可证
- 不要求具有许可证
支持文档
附加的软件/实用程序
安装到: Instrument
操作系统
- Windows 7
- Windows XP
- Windows 2000
- Windows NT
- Windows ME
前提要求
无
支持的仪器
- N8920A, N8921A, N8923A, N8924A, N8925A, N8926A, N8928A, N8929A, N8930A, N8931A, N8932A, N8934A, N8935A, N8937A, N8940A, N8941A, N8943A, N8944A, N8945A, N8946A, N8948A, N8949A, N8950A, N8951A, N8952A, N8954A, N8955A, N8957A
SHOW MORE