Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

M9393A PXIe Performance Vector Signal Analyzer Instrument Drivers

For a complete list of all instrument drivers from Keysight, please visit www.keysight.com/find/drivers

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only), LabVIEW (32-bit/64-bit)

IVI class support: IviDriver 1.0

LabVIEW driver version: 2.0.3

Version Description:

  • When the M9393A driver is initialized with “ExternalDigitizer=true” or “ExternalDigitizer=1” in the option string, M9214A IF Digitizer is no longer required in the PXI chassis.
  • A new M9393 wideband IF hardware extension for the 89600 VSA has been added that allows a M3993A to be paired with a M9203A digitizer to obtain measurement bandwidth up to 1 GHz.
  • New FPGA bits with improved stability.
Release Date Version Version Description
2017-05-25 2.1.910.2 See description above.

How to Download

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

How to Install

  • Run the downloaded installer.

Licensing

  • Does Not Require a License

Supporting Documentation

Download

Installs on:

PC

Operating System

  • Windows 8
  • Windows 7

Prerequisites

Supported Instruments

  • M9393A (modules supported: M9214A, M9308A, M9365A, M9169E)

Related Links