What are you looking for?
Suggested searches
No product matches found - System Exception
Matched content
89600 VSA Software DOCSIS 3.1 Configuration Wizard
Use the DOCSIS 3.1 configuration wizard to create the OFDM setup files for 89600 VSA custom OFDM (Option BHF) based on the downstream and upstream configurations.
These files are not available in the 89600 VSA software DVD or webhelp file.
Keysight empfiehlt die Verwendung der aktuellen Version, die die neuesten verfügbaren Fehlerbehebungen und Sicherheitspatches enthält.
Veröffentlichungsdatum | Version | Versionsbeschreibung |
---|---|---|
2015-10-06 | 1.4.6.0 | New feature: Modified menus of DOCSIS 3.1 upstream wizard with upper/lower guard subcarriers, additional setup file creation with SpanOptimized checkbox, and some defect fixes. |
Veröffentlichungsdatum | Version |
---|---|
2015-10-06 | 1.4.6.0 |
Version Description |
---|
New feature: Modified menus of DOCSIS 3.1 upstream wizard with upper/lower guard subcarriers, additional setup file creation with SpanOptimized checkbox, and some defect fixes. |
How to Download
- Click on the Download button
- Select Save
- Extract the files from the zip file to a folder on your hard drive
- Double-click on Setup-DOCSIS31-Wizard.msi to install the wizard
How to Install
See Supporting Documentation
Lizenzierung
- Does Not Require a License
Supporting Documentation
Installs on: PC
Operating System
- Windows 8 Professional
- Windows 8 Enterprise
- Windows 7 Professional
- Windows 7 Enterprise
- Windows 7 Ultimate
Voraussetzungen
Supported Instruments
How to Download
- Click on the Download button
- Select Save
- Extract the files from the zip file to a folder on your hard drive
- Double-click on Setup-DOCSIS31-Wizard.msi to install the wizard
How to Install
See Supporting Documentation
Lizenzierung
- Does Not Require a License
Supporting Documentation
Installs on: PC
Operating System
- Windows 8 Professional
- Windows 8 Enterprise
- Windows 7 Professional
- Windows 7 Enterprise
- Windows 7 Ultimate
Voraussetzungen
- 89600 VSA v18.5 or later to be installed, licensed with Options 200, 300 and BHF (required for the wizard to create Custom OFDM setup files for DOCSIS 3.1 formats)
Supported Instruments
How to Download
- Click on the Download button
- Select Save
- Extract the files from the zip file to a folder on your hard drive
- Double-click on Setup-DOCSIS31-Wizard.msi to install the wizard
How to Install
See Supporting Documentation
Lizenzierung
- Does Not Require a License
Supporting Documentation
Installs on: PC
Operating System
- Windows 8 Professional
- Windows 8 Enterprise
- Windows 7 Professional
- Windows 7 Enterprise
- Windows 7 Ultimate
Voraussetzungen
- 89600 VSA v18.5 or later to be installed, licensed with Options 200, 300 and BHF (required for the wizard to create Custom OFDM setup files for DOCSIS 3.1 formats)
Supported Instruments
How to Download
- Click on the Download button
- Select Save
- Extract the files from the zip file to a folder on your hard drive
- Double-click on DOCSIS31.exe to run the wizard
How to Install
See Supporting Documentation
Lizenzierung
- Does Not Require a License
Supporting Documentation
Installs on: PC
Operating System
- Windows 8 Professional
- Windows 8 Enterprise
- Windows 7 Professional
- Windows 7 Enterprise
- Windows 7 Ultimate
Voraussetzungen
- 89600 VSA v18 or later to be installed, licensed with Options 200, 300 and BHF (requiredfor thewizard to create Custom OFDM setup files for DOCSIS 3.1 formats)
Supported Instruments
- N9070A Wideband Signal Analysis Solutions
SHOW MORE