Use the DOCSIS 3.1 configuration wizard to create the OFDM setup files for 89600 VSA custom OFDM (Option BHF) based on the downstream and upstream configurations.

These files are not available in the 89600 VSA software DVD or webhelp file.

Keysight recommends using the most current version, which includes the most up-to-date bug fixes and security patches available.
Release Date Version Version Description
2015-10-06 1.4.6.0 New feature: Modified menus of DOCSIS 3.1 upstream wizard with upper/lower guard subcarriers, additional setup file creation with SpanOptimized checkbox, and some defect fixes.
Release Date Version
2015-10-06 1.4.6.0
Version Description
New feature: Modified menus of DOCSIS 3.1 upstream wizard with upper/lower guard subcarriers, additional setup file creation with SpanOptimized checkbox, and some defect fixes.

How to Download

  • Click on the Download button
  • Select Save
  • Extract the files from the zip file to a folder on your hard drive
  • Double-click on Setup-DOCSIS31-Wizard.msi to install the wizard

How to Install

  • See Supporting Documentation

Licensing

  • Does Not Require a License

Installs on: PC

Operating System

  • Windows 8 Professional
  • Windows 8 Enterprise
  • Windows 7 Professional
  • Windows 7 Enterprise
  • Windows 7 Ultimate

How to Download

  • Click on the Download button
  • Select Save
  • Extract the files from the zip file to a folder on your hard drive
  • Double-click on Setup-DOCSIS31-Wizard.msi to install the wizard

How to Install

  • See Supporting Documentation

Licensing

  • Does Not Require a License

Installs on: PC

Operating System

  • Windows 8 Professional
  • Windows 8 Enterprise
  • Windows 7 Professional
  • Windows 7 Enterprise
  • Windows 7 Ultimate

Prerequisites

  • 89600 VSA v18.5 or later to be installed, licensed with Options 200, 300 and BHF (required for the wizard to create Custom OFDM setup files for DOCSIS 3.1 formats)

How to Download

  • Click on the Download button
  • Select Save
  • Extract the files from the zip file to a folder on your hard drive
  • Double-click on Setup-DOCSIS31-Wizard.msi to install the wizard

How to Install

  • See Supporting Documentation

Licensing

  • Does Not Require a License

Installs on: PC

Operating System

  • Windows 8 Professional
  • Windows 8 Enterprise
  • Windows 7 Professional
  • Windows 7 Enterprise
  • Windows 7 Ultimate

Prerequisites

  • 89600 VSA v18.5 or later to be installed, licensed with Options 200, 300 and BHF (required for the wizard to create Custom OFDM setup files for DOCSIS 3.1 formats)

How to Download

  • Click on the Download­ button
  • Select Save
  • Extract the files from the zip file to a folder on your hard drive
  • Double-click on DOCSIS31.exe to run the wizard

How to Install

  • See Supporting Documentation

Licensing

  • Does Not Require a License

Installs on: PC

Operating System

  • Windows 8 Professional
  • Windows 8 Enterprise
  • Windows 7 Professional
  • Windows 7 Enterprise
  • Windows 7 Ultimate

Prerequisites

  • 89600 VSA v18 or later to be installed, licensed with Options 200, 300 and BHF (required­for the­wizard to create Custom OFDM setup files for DOCSIS 3.1 formats)

Supported Instruments

  • N9070A Wideband Signal Analysis Solutions
SHOW MORE