What are you looking for?
Suggested searches
No product matches found - System Exception
Matched content
Guide to Setup FieldFox Remote Keyboard Utility
The Remote Keyboard utility provides an alternate method to control FieldFox remotely, and it is used along with FieldFox Remote Display.
Usage note: Remote Keyboard Utility on this page is not officially supported by Keysight and do not have extensive error checking. It is provided as a convenience. The self-extracting zipped file must be executed to extract the installation file.
Installation Requirement:
- FieldFox Keyboard requires Keysight IO Libraries to work together. Go to www.keysight.com/find/iosuite and follow the links to install the free software.
- Establish a LAN connection between the FieldFox and the PC. When the connection is established you will have IP addresses for the FieldFox.
To use this remote keyboard utility:
- Download FieldFox_Keyboard.zip from below.
- Execute FieldFox_Keyboard from the folder. The FieldFox Remote Keyboard window will appear on the PC.
- Click Connect button at the bottom left of the user interface.
- Enter FieldFox IP address and click Connect. A window dialog will pop-up upon successful connection.
Keysight empfiehlt die Verwendung der aktuellen Version, die die neuesten verfügbaren Fehlerbehebungen und Sicherheitspatches enthält.
Veröffentlichungsdatum | Version | Versionsbeschreibung |
---|---|---|
2013-10-20 | 1.0 | Zip file contain FieldFox Remote Keyboard setup file |
Veröffentlichungsdatum | Version |
---|---|
2013-10-20 | 1.0 |
Version Description |
---|
Zip file contain FieldFox Remote Keyboard setup file |
How to Download
Click the download button, select file, save and unzip.
How to Install
Please read the installation instruction guide from above.
Lizenzierung
- Does Not Require a License
Installs on: PC
Operating System
- Other Windows
Voraussetzungen
- FieldFox Keyboard requires Agilent IO Libraries to work together. Go to www.agilent.com/find/iosuite and follow the links to install the free software.
- LAN connection between FieldFox and PC.
Supported Instruments
- N9912A, N9923A, N9913A, N9914A, N9915A, N9916A, N9917A, N9918A, N9925A, N9926A, N9927A, N9928A, N9935A, N9936A, N9937A, N9938A
Keine Softwareversion verfügbar
SHOW MORE