是德建议使用最新的版本,其中包括最新的漏洞修复和安全补丁
免运费 Trial
发布日期 版本 版本说明
2016-11-10 3.2.0.30373 Waveform Creator Version 3.2
发布日期 版本
2016-11-10 3.2.0.30373
版本说明
Waveform Creator Version 3.2

The M9099 Waveform Creator is a modular software application focused on easy development of complex baseband and vector signals used in the validation and test of digital communications products. Built around a “drag and drop” graphical user interface, Waveform Creator allows quick development of multi-format, multi-track waveforms with waveform segments displaced in frequency and time.

Waveform Creator 3.2 adds the following key features:

  • Carrier Summing Enhancements in Track Alignment.
  • Additional Marker types
    • Period/Length Pair
    • ALC from Highest Power Track
    • Auto Generated RF Blanking
  • “ALC On/Off” and marker routing setting for “RF Blanking” and “ALC Hold” for MXG/ESG/EXG output device.
  • FSK filter for Digital Modulation 2-FSK/4-FSK/8-FSK/16-FSK.
  • Transmit OSR” and Granularity Options for M8190A.
  • Ability to download “Specified Segment IDs” and “Waveform Caching” support to the M8190A.
  • SCPI commands for creating user defined Pre-Correction for M8190A.
  • Pre-Correction when using the “File” Output Device.

如何下载

  • Click the Download button
  • Select Run
  • Follow the screen prompts to install the software.

颁发许可证

  • 要求具有许可证

安装到: PC

操作系统

  • Windows 7

支持的仪器

  • 33522 (AWG), 33600 (AWG), 81180A/B, 89600 (VSA Simulation Output), E4438C (ESG), M8190A, M8195A (AWG), M9330/31A, M9381A, N5172B (EXG), N5182A/B (MXG), and N824xA (AWG)

The M9099 Waveform Creator is a modular software application focused on easy development of complex baseband and vector signals used in the validation and test of digital communications products. Built around a “drag and drop” graphical user interface, Waveform Creator allows quick development of multi-format, multi-track waveforms with waveform segments displaced in frequency and time.

Waveform Creator 3.1 adds the following key features:

  • Added Digital Modulation support for APCO25 Phase1 - C4FM, Phase1 - CQPSK, Tetra-1 and ARIB T98/61/102
  • Updated DOCSIS 3.1 upstream signal generation capabilities.
  • Added QAM 2048 and 4096 in Digital Modulation plug-in
  • Added Dual Sine Wave to Basic Waveform plug-in
  • Expanded lower waveform frequency limit from 100 kHz to 1 Hz
  • Added “Sequencing Mode” and “Dynamic Control On” to M8190A dynamic sequencer
  • Added support for Keysight 33522 & 33600 series AWG

如何下载

  • Click the Download button
  • Select Run
  • Follow the screen prompts to install the software.

颁发许可证

  • 要求具有许可证

安装到: PC

操作系统

  • Windows 7

支持的仪器

  • 33522 (AWG), 33600 (AWG), 81180A/B, 89600 (VSA Simulation Output), E4438C (ESG), M8190A, M8195A (AWG), M9330/31A, M9381A, N5172B (EXG), N5182A/B (MXG), and N824xA (AWG)

The M9099 Waveform Creator is a modular software application focused on easy development of complex baseband and vector signals used in the validation and test of digital communications products. Built around a “drag and drop” graphical user interface, Waveform Creator allows quick development of multi-format, multi-track waveforms with waveform segments displaced in frequency and time.

Waveform Creator 3.1 adds the following key features:

  • Added QAM 2048 and 4096 in Digital Modulation plug-in
  • Added prefix symbols for upstream DOCSIS
  • Added new payload formats (From Text File: 1 bit per line and Sequential 1/0 data )
  • Changed default FSK Frequency Deviation from 10 kHz to 8 MHz
  • Support downloading encrypted waveforms to M8190A (remote and direct)
  • Updated DOCSIS to support DOCSIS Configuration Wizard v1.4.7.0
  • Added support for N824xA DDS mode
  • Added Dual Sine Wave to Basic Waveform plug-in
  • Expanded lower waveform frequency limit from 100 kHz to 1 Hz
  • Added “ARB ON” and “PlayARB n” to match M9381A SFP
  • Added “Sequencing Mode” and “Dynamic Control On” to M8190A dynamic sequencer
  • Support Single Channel waveform download to M8190A
  • Added support for the following Keysight products:
    • 33522 Series AWG
    • 33600 Series AWG

如何下载

  • Click the Download button
  • Select Run
  • Follow the screen prompts to install the software.

颁发许可证

  • 要求具有许可证

安装到: PC

操作系统

  • Windows 7

支持的仪器

  • 33522 (AWG), 33600 (AWG), 81180A/B, 89600 (VSA Simulation Output), E4438C (ESG), M8190A, M8195A (AWG), M9330/31A, M9381A, N5172B (EXG), N5182A/B (MXG), and N824xA (AWG)

The M9099 Waveform Creator is a modular software application focused on easy development of complex baseband and vector signals used in the validation and test of digital communications products. Built around a “drag and drop” graphical user interface, Waveform Creator allows quick development of multi-format, multi-track waveforms with waveform segments displaced in frequency and time. Its modularity supports multiple waveform types and VSG/AWG instruments to be “plugged in”, supporting expansion to include both current & future waveform types and instruments.

Waveform Creator 3.0 provides the following key features:

  • Optional generation of DOCSIS 3.1 downstream and upstream signals.
  • Optional waveform creation plug-in for basic digital modulation.
  • Optional waveform creation plug-in for SystemVue simulation models.
  • Other Standard waveform plug-ins for general-purpose waveform creation.
  • Importing of waveform data from CSV, LabVIEW CSV, HDF, BIN,
  • M8190A DUC IQBINFile, or Signal Studio's WFM file type.
  • Flexible waveform creation and generation capability for the following Keysight products:
    • M9381A PXI VSG,
    • N5182A/B MXG, N5172B EXG, and E4438C ESG,
    • M933xA AWG, N824xA AWG, and
    • M8195A AWG, M8190A AWG and 81180A/B AWG
  • Output plug-in for writing unencrypted waveform files (CSV, MAT,BIN,M8190A
  • DUC IQBIN, M9381A native files, and WFM).
  • User extendable functionality such as creating your own waveform input plug-ins.
  • SCPI remote control for test automation.

如何下载

  • Click the Download button
  • Select Run
  • Follow the screen prompts to install the software.

颁发许可证

  • 要求具有许可证

安装到: PC

操作系统

  • Windows 7

支持的仪器

  • M9381A, M8190A, 81180A/B, M9330/31A N5182A/B (MXG), N5172B (EXG), E4438C (ESG), M8195A (AWG), N824xA (AWG), and 89600 (VSA Simulation Output)

The M9099 Waveform Creator is a modular software application focused on easy development of complex baseband and vector signals used in the validation and test of digital communications products. Built around a “drag and drop” graphical user interface, Waveform Creator allows quick development of multi-format, multi-track waveforms with waveform segments displaced in frequency and time. Its modularity supports multiple waveform types and VSG/AWG instruments to be “plugged in”, supporting expansion to include both current & future waveform types and instruments.

如何下载

  • Click the Download button
  • Select Run
  • Follow the screen prompts to install the software.

颁发许可证

  • 要求具有许可证

支持文档

安装到: PC

操作系统

  • Windows 7

前提要求

支持的仪器

  • M9381A, M8190A, 81180A/B, M9330/31A

The M9099 Waveform Creator is a modular software application focused on easy development of complex baseband and vector signals used in the validation and test of digital communications products. Built around a “drag and drop” graphical user interface, Waveform Creator allows quick development of multi-format, multi-track waveforms with waveform segments displaced in frequency and time. Its modularity supports multiple waveform types and VSG/AWG instruments to be “plugged in”, supporting expansion to include both current & future waveform types and instruments.

如何下载

  • Click the Download button
  • Select Run
  • Follow the screen prompts to install the software.

颁发许可证

  • 要求具有许可证

支持文档

安装到: PC

操作系统

  • Windows 7

前提要求

支持的仪器

  • M9381A
SHOW MORE