您希望搜索哪方面的内容?
N4980A 多仪器 BERT 软件
N4980A 多仪器 BERT 软件可以为下列仪器提供易于使用的控制面板:
Keysight | Centellax |
---|---|
N4960A 串行 BERT 32 和 17 Gb/s | SSB16000 |
N4962A 串行 BERT 12.5 Gb/s | TG1B1A |
N4963A 时钟合成器 13.5 Gb/s | TG2C1A |
N4965A 多通道 BERT 12.5 Gb/ | PCB12500 |
N4971A 码型发生器 13 Gb/s | PPG12500 |
N4972A 时钟合成器 16 GHz | SCS16000 |
N4980A-JTS 抖动容量测量套件是一款使用软件密匙的选件。
发布日期 | 版本 | 版本说明 |
---|---|---|
2015-02-18 | 3.3.2905 | Adds support for Keysight branded instruments. |
发布日期 | 版本 |
---|---|
2015-02-18 | 3.3.2905 |
版本说明 |
---|
Adds support for Keysight branded instruments. |
如何下载
- Click the Download button
- Save the software to your PC
如何安装
颁发许可证
- 不要求具有许可证
支持文档
安装到: PC
操作系统
- Windows 7 (32-bit) (English or Chinese)
- Windows 7 (64-bit) (English)
- Windows 10 (32-bit)
- Windows 10 (64-bit)
前提要求
支持的仪器
- N4960A, N4962A, N4963A, N4965A, N4971A, N4972A
相关链接
如何下载
- Click the Download button
- Save the software to your PC
如何安装
颁发许可证
- 不要求具有许可证
支持文档
安装到: PC
操作系统
- Windows 7 32-bit (English or Chinese)
- Windows 7 64-bit (English)
前提要求
- PC: Intel Pentium processor or equivalent
- Screen Resolution: XGA+ 1152x864 (min)
- RAM: 500 MB (min); 4 GB (min for Windows 7 64-bit)
- Disk space for installation: 100 MB
- .NET framework version 3.5
- I/O Libraries (for GPIB, not required for USB)
支持的仪器
- N4960A, N4962A, N4963A, N4965A, N4971A, N4972A
相关链接
如何下载
- 点击下载按钮
- 把软件保存到 PC
如何安装
颁发许可证
- 不要求具有许可证
支持文档
安装到: PC
操作系统
- Windows XP 32-bit (with SP3)
- Windows 7 32-bit (English or Chinese)
- Windows 7 64-bit (English)
前提要求
- PC:英特尔奔腾处理器或同档处理器
- 屏幕分辨率:1024x768(最低)
- RAM:500 MB(最低)
- 安装所需的空间: 100 MB
支持的仪器
- N4960A, N4962A, N4963A, N4965A, N4971A, N4972A
相关链接
如何下载
- Download the software into the PC.
- Please read the N4980A Getting Started Guide before installing the software.
如何安装
颁发许可证
- 不要求具有许可证
支持文档
安装到: PC
操作系统
- Windows XP 32-bit (with SP3)
- Windows 7 32-bit (English or Chinese)
- Windows 7 64-bit (English)
前提要求
- PC: Intel Pentium processor or equivalent
- Screen Resolution: 1024x768 (min)
- RAM: 500 MB (min)
- Disk space for installation: 100 MB
- I/O Libraries
支持的仪器
- N4960A, N4962A, N4963A, N4965A, N4971A, N4972A
相关链接
The N4980A is dependent upon low level Virtual Instrument Software Architecture (VISA), such as the Keysight I/O libraries. If the PC onto which the N4980A will be installed already has Keysight I/O libraries installed, then they do not need to be installed again.
For communicating with instruments via USB, the FTDI VCP driver must be installed. If this is not automatically installed by the Windows OS via Plug And Play, it must be manually installed by the user. The FTDI VCP driver can be found at www.ftdichip.com/Drivers/VCP.htm.
如何下载
- Download the software into the PC.
- Please read the N4980A Getting Started Guide before installing the software.
如何安装
- See Documentation
颁发许可证
- 不要求具有许可证
支持文档
安装到: PC
操作系统
- Windows XP 32-bit (with SP3)
- Windows 7 32-bit (English or Chinese)
- Windows 7 64-bit (English)
前提要求
- PC: Intel Pentium processor or equivalent
- Screen Resolution: 1024x768 (min)
- RAM: 500 MB (min)
- Disk space for installation: 100 MB
- I/O Libraries
支持的仪器
- N4960A, N4962A, N4963A, N4965A, N4971A, N4972A
相关链接
The N4980A is dependent upon low level Virtual Instrument Software Architecture (VISA), such as the Keysight I/O libraries. If the PC onto which the N4980A will be installed already has Keysight I/O libraries installed, then they do not need to be installed again.
For communicating with instruments via USB, the FTDI VCP driver must be installed. If this is not automatically installed by the Windows OS via Plug And Play, it must be manually installed by the user. The FTDI VCP driver can be found at www.ftdichip.com/Drivers/VCP.htm.
如何下载
- Download the software into the PC.
- Please read the N4980A Getting Started Guide before installing the software.
如何安装
- See Documentation
颁发许可证
- 不要求具有许可证
支持文档
安装到: PC
操作系统
- Windows XP 32-bit (with SP3)
- Windows 7 32-bit (English or Chinese)
- Windows 7 64-bit (English)
前提要求
- PC: Intel Pentium processor or equivalent
- Screen Resolution: 1024x768 (min)
- RAM: 500 MB (min)
- Disk space for installation: 100 MB
- I/O Libraries
支持的仪器
- N4960A, N4962A, N4963A, N4965A, N4971A, N4972A
相关链接
The N4980A is dependent upon low level Virtual Instrument Software Architecture (VISA), such as the Keysight I/O libraries. If the PC onto which the N4980A will be installed already has Keysight I/O libraries installed, then they do not need to be installed again.
For communicating with instruments via USB, the FTDI VCP driver must be installed. If this is not automatically installed by the Windows OS via Plug And Play, it must be manually installed by the user. The FTDI VCP driver can be found at www.ftdichip.com/Drivers/VCP.htm.
如何下载
- Download the software into the PC.
- Please read the N4980A Getting Started Guide before installing the software.
如何安装
- See Documentation
颁发许可证
- 不要求具有许可证
支持文档
安装到: PC
操作系统
- Windows XP 32-bit (with SP3)
- Windows 7 32-bit (English or Chinese)
- Windows 7 64-bit (English)
前提要求
- PC: Intel Pentium processor or equivalent
- Screen Resolution: 1024x768 (min)
- RAM: 500 MB (min)
- Disk space for installation: 100 MB
- I/O Libraries
支持的仪器
- N4960A, N4962A, N4963A, N4965A, N4971A, N4972A