TS-5000 Version 7 Patches and Hotfixes for Windows 7 32-bit, Windows 7 64-bit and Windows XP 32-bit

Keysight empfiehlt die Verwendung der aktuellen Version, die die neuesten verfügbaren Fehlerbehebungen und Sicherheitspatches enthält.
Veröffentlichungsdatum Version Versionsbeschreibung
2018-11-28 7.1.9 TS-5000 version 7.1 Service Pack 9
Veröffentlichungsdatum Version
2018-11-28 7.1.9
Version Description
TS-5000 version 7.1 Service Pack 9

Release summary:

  • Bug fix for detecting invalid/defective load card in SysConfig.exe. It will show unknown when defective load cards are detected.
  • Update test limit for VI in CEDGN U8989A.tpa and CEDGN U8972A.tpa.
  • Action Enhancement: Widen speed and resolution selection for M918x DMM’s dmeasdcv.umd action
     

How to Download

  • Please click on the Download button to download the patch.

How to Install

  • Please double click on the file setup.exe or right click the file setup.exe and select run

Lizenzierung

  • Does Not Require a License

Installs on: PC

Operating System

  • Windows 7 32-bit
  • Windows 7 64-bit
  • Windows XP 32-bit

Voraussetzungen

  • Information Not Available

Supported Instruments

  • Entire TS-5400 family includes TS-5020, TS-5030, TS-5400 PXI, TS-5400, TS-5410, and TS-8989

The TS-5000 libraries version 7.1 Service Pack 8 is mainly for Keysight rebrand and added few instrument in our library and. For full details, please refer to the ReadMe.txt in the installation folder.

How to Download

  • Please click on the Download button to download the patch.

How to Install

  • Please double click on the file setup.exe or right click the file setup.exe and select

Lizenzierung

  • Does Not Require a License

Installs on: PC

Operating System

  • Windows 7 32-bit
  • Windows 7 64-bit
  • Windows XP 32-bit

Voraussetzungen

  • TestExec SL ver. 7.1.4 (or greater) must be installed prior to the installation of this patch.

Supported Instruments

  • Entire TS-5400 family includes TS-5020, TS-5030, TS-5400 PXI, TS-5400, TS-5410, and TS-8989

The TS-5000 libraries version 7.1.5 patch contains enhancements and bug fixes.  For full details, please refer to the ReadMe.txt in the installation folder.

How to Download

  • Please click on the Download button to download the patch.

How to Install

please double click on the file setup.exe or right click the file setup.exe and select

Lizenzierung

  • Does Not Require a License

Installs on: PC

Operating System

  • Windows 7
  • Windows Vista
  • Windows XP SP3
  • Windows XP SP2

Voraussetzungen

  • TestExec SL ver. 7.1.3 and TS-5000 ver. 7.1.0 or 7.1.1 must be installed prior to the installation of this patch.

Supported Instruments

  • TS-5040, TS-5020, TS-8989, TS-8900, TS-5400 PXI, TS-5400

The TS-5000 libraries version 7.1.4 patch contains enhancements and bug fixes.  For full details, please refer to the readme.txt in the installation folder.

How to Download

  • Please click on the Download button to download the patch.

How to Install

  • please double click on the file setup.exe or right click the file setup.exe and select

Lizenzierung

  • Does Not Require a License

Installs on: PC

Operating System

  • Windows 7
  • Windows Vista
  • Windows XP SP3
  • Windows XP SP2

Voraussetzungen

  • Test Exec SL version 7.1.3 and TS-5000 libraries version 7.1.0 must be installed prior to TS-5000 libraries version 7.1.4 installed.

Supported Instruments

  • TS-5040, TS-5020, TS-5400, TS-8900, TS-5400 PXI, TS-8989

This TS-5000 libraries version 7.1.3 includes patches and enhancements.  For full details of the patches and enhancements, please refer to the ReadMe.txt in the TS5000 7.1 Service Pack 3.zip file.

How to Download

  • Click on the download button.

How to Install

  • Extract the zip file downloaded and run the Setup.exe file

Lizenzierung

  • Does Not Require a License

Installs on: PC

Operating System

  • Windows 7
  • Windows Vista
  • Windows XP SP3
  • Windows XP SP2
  • Windows XP

Voraussetzungen

  • Information Not Available

Supported Instruments

  • TS-5040, TS-5020, TS-5400, TS-8900, TS-5400 PXI

This TS-5000 libraries version 7.1.2 provides enhancements and bug fixes. For more details on the enhancements and bug fixes, please refer to the Readme file inside the installer

How to Download

  • Click on the download button.

How to Install

  • Unzip the file TS5000_7.1_ServicePack2.zip and run setup.exe

Lizenzierung

  • Does Not Require a License

Installs on: PC

Operating System

  • Windows 7
  • Windows XP SP3
  • Windows XP SP2
  • Windows XP

Voraussetzungen

  • Please install TS-5000 7.1.0V or TS-5000 7.1.1.1V prior to installing TS-5000 7.1.2v. �Please do not apply TS-5000 7.x Hotfix patch after installing TS-5000 7.1.2
    This service pack includes files for 7.x Hotfix.

Supported Instruments

  • Not applicable

How to Download

  • Click on download button.

How to Install

  • Unzip downloaded file and run setup.exe.

Lizenzierung

  • Does Not Require a License

Minor Updates

Installs on: PC

Operating System

  • Windows 7

Voraussetzungen

  • TS 5000 7

Supported Instruments

  • Not Applicable

How to Download

  • Click on download button.

How to Install

  • Unzip downloaded file and run setup.exe.

Lizenzierung

  • Does Not Require a License

Minor Updates

Installs on: PC

Operating System

  • Windows 7

Voraussetzungen

  • TS 5000 7

Supported Instruments

  • Not Applicable
SHOW MORE