这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家联系

X 系列信号分析仪 LTE FDD IVI 和 MATLAB 仪器驱动程序

For a complete list of all instrument drivers from Keysight, please visit www.keysight.com/find/drivers

This driver download installs the IVI-C, IVI-COM, and MATLAB driver components.

Keysight instrument drivers also require that Keysight IO Libraries Suite be installed. To get the latest release of the IO Libraries Suite, go to www.keysight.com/find/iosuite

Current Version Details
Version 1.0.7.0
Models Supported N9010A, N9020A, N9030A
IO Libraries Required Version 16.0 or greater
Driver Types and Version IVI-C (32-bit/64-bit)
IVI-COM (32-bit/64-bit)
MATLAB (32-bit/64-bit)
IVI Classes Supported IviDriver 1.0
Minimum IVI Shared Components Version 2.2.1.0 


 

发布日期 版本 版本说明
2015-12-05 1.0.10.0 Added index 13 to 17 to the SEM measurement.

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only)

IVI class support: IviDriver 1.0

IVI Generation: IVI-2014

如何下载

  1. Click the Download button
  2. Select the appropriate executable file
  3. Choose Run

如何安装

  • Run the downloaded installer

颁发许可证

  • 不要求具有许可证

支持文档

2015-01-16 1.0.9.0 See description below.

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only)

IVI class support: IviDriver 1.0

IVI Generation: IVI-2014

Version Description:

  • Updated help file
  • Added IVI-2014 Compliance
  • Rebranded as Keysight Technologies
  • Bug Fix: Previous versions of this driver contained COM GUID's that conflicted with the AgilentSAn IVI driver. If both drivers were installed, the drivers could become unusable. This issue has been fixed by replacing the conflicting COM GUID's in this driver.

如何下载

  1. Click the Download button
  2. Select the appropriate executable file
  3. Choose Run

如何安装

  • Run the downloaded installer

颁发许可证

  • 不要求具有许可证

支持文档

2012-07-02 1.0.7.0 This instrument driver provides access to the functionality of N9010A, N9020A, N9030A through a COM server or ANSI C API which also complies with the IVI specifications. Updated February 20, 2013 with digitally signed downloads.

如何下载

  1. Click the Download button
  2. Select the appropriate executable file
  3. Choose Run

如何安装

  • Run the downloaded installer

颁发许可证

  • 不要求具有许可证

支持文档