이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

IO Libraries Suite Downloads

To find out more about the IO Libraries Suite, visit www.keysight.com/find/iosuite

IO Libraries Suite 2017 includes the following features:

  • Fixed several stability issues that could cause Connection Expert to crash.
  • Fixed an issue where LAN connections would open twice as many sockets as needed.
  • Fixed an issue where aliases didn’t work on all PXI addresses.
  • Fixed an issue where PXI configuration.ini was reset to defaults during installation.
  • Added the ability to set the Method to “User Selected” for the PXI Resource Manager.
  • See readme for complete list of defect fixes
릴리스 날짜 버젼 버전 설명
2017-06-14 2017 Update 1 See description above. Build 18.0.22209.2

다운로드 방법

  • Click the download link and save the installer.

설치 방법

  • Run the downloaded installer.

라이센스

  • 라이센스 필요 없음

지원 문서

다운로드

설치 위치:

PC

운영 체제

  • Windows 10
  • Windows 8.1
  • Windows 7 SP1
  • Windows Server 2012 (64-bit only)
  • Windows Server 2008 R2 SP1 (64-bit only)

사전 조건

  • No specific prerequisites

지원되는 계측기

  • All instruments.

관련 링크