Here’s the page we think you wanted. See search results instead:

 

Sprechen Sie mit einem Experten

E5500 Phase Noise Measurement System Software

Release Date Version Version Description
2015-06-30 A.04.05.0010 Resolved known issues.

How to Download

  • Current E5500A software A.04.05.0010
    ◦  Navigate to the Windows Control Panel and uninstall:
       - E5500A Prerequisites
       - Agilent Host Processor Platform   
       - Agilent IO Libraries
       - All the files in the NI folder
       - IVI Shared Components
       - VISA Shared Components
    ◦  Download and install;
       - E5500_Prerequisites_A.01.02.exe
       - E5500_Installer_A.04.05.0010.exe 
     
  • Users who need to use the software in a computer that does not control instruments and only need the ability to view .pnm files should download the E5500_Installer also, by selecting the “Download” button. You do not need to download the Prerequisites file to view .pnm files.
  • Note: To disable the demo mode, click on System > Asset Manager > DM button on the tool bar
     

How to Install

  • See "How to Download"

Licensing

  • Does Not Require a License

Supporting Documentation

Download

Installs on:

Instrument

Operating System

  • Windows XP SP3
  • Windows 7 (32 bit)
  • Not for use with Windows 7 (64 bit)
  • Not for use with Windows 2000
  • Not for use with Windows NT
  • Note: Do not use with II PCI20428W-1 digitizer

Prerequisites

Supported Instruments

  • E5501A, E5501B, E5502A, E5502B, E5503A, E5503B, E5504A, E5504B, E5505A

Related Links