这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家联系

X 系列信号分析仪 IVI 和 MATLAB 仪器驱动程序

For a complete list of all instrument drivers from Keysight, please visit
www.keysight.com/find/drivers

This driver download installs the IVI-C, IVI-COM, and MATLAB driver components.

Keysight instrument drivers also require that Keysight IO Libraries Suite be installed. To get the latest release of the IO Libraries Suite, go to www.keysight.com/find/iosuite
 

Current Version Details
Version 2.0.0.0
Models Supported N9000A, N9010A, N9020A, N9030A, N9038A
IO Libraries Required Version 16.0 or greater
Driver Types and Version IVI-C (32-bit/64-bit)
IVI-COM (32-bit/64-bit)
MATLAB (32-bit/64-bit)
IVI Classes Supported IviSpecAn 1.0
IviLxiSync 1.0
IviDriver 1.0
Minimum IVI Shared Components Version 2.1.1.0 
发布日期 版本 版本说明
2017-03-07 3.4.2.0 Added support for N9041B, added System Preset, Global Center Freq, Extended Low Band, and External Trigger Compensation functionality. Fixed an issue where the driver would fail to install if the help file could not be installed.

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only)

IVI class support: IviDriver 1.0, IviSpecAn 2.0
 

如何下载

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

如何安装

  • Run the downloaded installer.

颁发许可证

  • 不要求具有许可证

支持文档

下载

安装于:

PC

操作系统

  • Windows 8
  • Windows 7
  • Windows 10

前提条件

支持的仪器

  • N9000A, N9000B, N9010A, N9010B, N9020A, N9020B, N9030A, N9030B, N9038A, M9290A, N9040B, N9041B, M9420A, M9421A, PN9003A, SPN9026A, N8973B, N8974B, N8975B, N8976B

相关链接

2016-06-02 3.3.0.0 Adds support for the M9421A.

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only)

IVI class support: IviDriver 1.0, IviSpecAn 2.0
 

如何下载

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

如何安装

  • Run the downloaded installer.

颁发许可证

  • 不要求具有许可证

支持文档

下载

安装于:

PC

操作系统

  • Windows 8
  • Windows 7
  • Windows 10

前提条件

支持的仪器

  • N9000A, N9000B, N9010A, N9010B, N9020A, N9020B, N9030A, N9030B, N9038A, M9290A, N9040B, M9420A, M9421A, PN9003A, SPN9026A, N8973B, N8974B, N8975B, N8976B

相关链接

2016-01-05 3.2.3.0 Model support added for N9000B,N9010B, N9020B, N9030B, SPN9003A, SPN9026A, N8973B, N8974B, N8975B, N8976B.

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only)

IVI class support: IviDriver 1.0, IviSpecAn 2.0
 

如何下载

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.
     

如何安装

  • Run the downloaded installer.

颁发许可证

  • 不要求具有许可证

支持文档

下载

安装于:

PC

操作系统

  • Windows 8
  • Windows 7
  • Windows Vista
  • Windows XP

前提条件

支持的仪器

  • N9000A N9000B N9010A N9010B N9020A N9020B N9030A N9030B N9038A M9290A N9040B M9420A SPN9003A SPN9026A N8973B N8974B N8975B N8976B

相关链接

2015-11-03 3.1.2.0 Implementation of IAgXSAnSystem.GetScreenImage method is modified to store the Screen.png file at D: incase of firmware version A.14 or earlier and to C:Temp incase of firmware version A.15 and later.

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only)

IVI class support: IviDriver 1.0, IviSpecAn 2.0

如何下载

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

如何安装

  • Run the downloaded installer.

颁发许可证

  • 不要求具有许可证

支持文档

2015-10-28 3.1.1.0 See description above.

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only)

IVI class support: IviDriver 1.0, IviSpecAn 2.0

Version description:

  • Customer issue fixed by changing the implementation of IAgXSAnInputRf.Coupling, removed the option checking and made equivalent to version before 3.0.0.0. Any option issue would be reported as error.
  • Customer issue fixed by changing the implementation logic of the IAgXSAnCalibration.Calibrate() method to read the status of calibration before returning, and increased the timeout to 240 seconds to cater to any delays or long calibration turnaround time.
  • Modified the implementation logic of the Initialze method for M9420A and M9290A modules, in case of PXI address, it check for module name and then take the correct installation path of LaunchModularSA.exe path based on the module name.
  • IVI-C issue fixed for some functions which take a Null value as an input.
  • Implementation of IAgXSAnSystem.GetScreenImage method is modified to remove the D: drive from the path.
  • Added trace numbers from 13 to 17 in SEMAsk measurement. Now user can access traces from 13 to 17.
     

如何下载

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.
     

如何安装

  • Run the downloaded installer

颁发许可证

  • 不要求具有许可证

支持文档

2015-07-21 3.1.0.0 Added support for M9420A.

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only)

IVI class support: IviDriver 1.0, IviSpecAn 2.0

如何下载

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.
     

如何安装

  • Run the downloaded installer

颁发许可证

  • 不要求具有许可证

支持文档

2015-04-18 3.0.0.0 Tracking Generator support added to N9000A and M9290A models.

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only)

IVI class support: IviDriver 1.0, IviSpecAn 2.0
 

如何下载

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

如何安装

  • Run the downloaded installer

颁发许可证

  • 不要求具有许可证

支持文档

2014-11-21 2.2.1.0 Rebranded Keysight Technologies, added support of UXA (N9040B) and CXA-m (M9290A).

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only)

IVI class support: IviDriver 1.0, IviSpecAn 2.0

IVI Generation: IVI-2014

如何下载

  1. Click the Download button.
  2. Select the appropriate executable file. 
  3. Choose Run.

如何安装

  • Run the downloaded installer

颁发许可证

  • 不要求具有许可证

支持文档

2014-04-26 2.1.4.0 Changed the implementation of the IAgXSAnCalibration.Calibrate method to increase the timeout of :CALibration[:ALL] SCPI.

如何下载

  1. Click the Download button.
  2. Select the appropriate executable file. 
  3. Choose Run.

如何安装

  • Run the downloaded installer

颁发许可证

  • 不要求具有许可证

支持文档

2014-01-06 2.1.3.0 Fixed an application crash when calling init function (IVI-COM or IVI-C) if you use an address where there is no instrument available (e.g. instrument is turned off or LAN cable is disconnected).

如何下载

  1. Click the Download button.
  2. Select the appropriate executable file. 
  3. Choose Run.

如何安装

  • Run the downloaded installer

颁发许可证

  • 不要求具有许可证

支持文档

2013-06-26 2.1.2.0 Defect fixes and system interface revised for adding ClearIO, ReadByte(),WriteByte(),ReadString(),WriteString() methods

如何下载

  1. Click the Download button.
  2. Select the appropriate executable file. 
  3. Choose Run.

如何安装

  • Run the downloaded installer

颁发许可证

  • 不要求具有许可证

支持文档

2011-05-24 2.0.0.0 Applied updated policy. No functionality change.

如何下载

  • 1. Click the Download button. 2. Select the appropriate executable file. 3. Choose Run.

如何安装

  • See Readme File

颁发许可证

  • 不要求具有许可证

支持文档

2011-05-10 1.0.5.0 Initial public release.

如何下载

  • 1. Click the Download button. 2. Select the appropriate executable file. 3. Choose Run.

如何安装

  • See Readme File

颁发许可证

  • 不要求具有许可证

支持文档