这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家联系

M9018A 18 插槽 PXIe 机箱驱动程序

For a complete list of all instrument drivers from Keysight, please visit www.keysight.com/find/drivers

This driver download installs the IVI-C, IVI-COM, LabVIEW, and MATLAB driver components, as well as the soft front panel and kernel device driver.

Keysight modular drivers also require that Keysight IO Libraries Suite 16.0 or greater be installed. To get the latest release of the IO Libraries Suite, go to www.keysight.com/find/iosuite

Current Version Details
Version 1.2.3
Models Supported M9018A
IO Libraries Required Version 16.2 or greater
Driver Types and Version IVI-C (32/64-bit) 1.2.1.3
IVI-COM (32/64-bit) 1.2.1.3
LabVIEW (32/64-bit) 1.0.5
MATLAB (32-bit) 1.2.1.3
Soft Front Panel Version 1.2.1.3
IVI Classes Supported IviDriver 1.0
Minimum IVI Shared Components Version 2.1.1 
发布日期 版本 版本说明
2016-09-04 1.6.2.1 See description below.

This package installs 2 drivers:

KtMPxiChassis Driver

  • Driver type: IVI-C (32-bit/64-bit), IVI.NET (32-bit/64-bit), LabVIEW (32-bit/64-bit)
  • IVI-C class support: IviDriver 2.1
  • IVI.NET class support: IviDriver 1.0
  • LabVIEW driver version: 1.0.1
  • Version description:
    • Initial release
    • Supports M9019A

Legacy AgM9018 Driver

  • Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only), LabVIEW (32-bit/64-bit)
  • IVI class support: IviDriver 1.0
  • LabVIEW driver version: 1.1.5
  • Version description:
    • New feature added: Trigger Manager for managing trigger resources to prevent conflicts between applications. The AgM9018 IVI driver API has not changed, however, trigger routing done through the AgM9018 driver is now subject to PXI-9 Trigger Manager rules which can result in errors indicating a conflict between applications.
    • Supports M9018A

如何下载

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

如何安装

  • Run the downloaded installer.

颁发许可证

  • 不要求具有许可证

支持文档

2015-02-05 1.5.80.1 See description below.

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only), LabVIEW (32-bit/64-bit)

IVI class support: IviDriver 1.0

LabVIEW driver version: 1.2.6

Version description:

  • Changes made to support the HP Z440/640/840 series of controllers
  • Visual Studio examples updated to use Visual Studio 2010 (or later)
  • Document changes to meet IVI-2014 Compliance
  • Rebranded as Keysight Technologies

如何下载

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

如何安装

  • Run the downloaded installer.

颁发许可证

  • 不要求具有许可证

支持文档

2014-10-28 1.4.397.1 See description below.

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only), LabVIEW (32-bit/64-bit)

IVI class support: IviDriver 1.0

LabVIEW driver version: 1.0.5

Version description:

  • Updated to Rev 2 of 2x8 and 4x4 PCIe fabrics.
  • Default fan alarm level raised from 800 rpm to 1200 rpm.
  • Eliminated use of English-language dependent string in System Module DLL.
  • Eliminated driver 1st-contact SMBus self test operations to improve interoperability.

如何下载

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

如何安装

  • Run the downloaded installer.

颁发许可证

  • 不要求具有许可证

支持文档

2013-07-19 1.3.443.1 Updated PXI System Module DLL and Chassis Driver DLL to support cascaded multi-chassis systems. Added 1x8 PCIe Gen1 speed fabric to PCIe Switch Fabric Configurator (for use with multi-chassis systems).

如何下载

  1. Click the Download button.
  2. Select the appropriate executable file. 
  3. Choose Run.

如何安装

  • Run the downloaded installer.
  • If you see a Windows Security prompt, check the box Always trust software from "Agilent Technologies, Incorporated", then click the Install button to install the driver.

颁发许可证

  • 不要求具有许可证

支持文档

2012-03-22 1.2.3 Added support for 2-Link 2x8 PCIe Switch Fabric, added support for Keysight IO Libraries 16.2, fixed assorted PXI compliance issues (updated System Module DLL, Chassis DLL, and Chassis Description file)

如何下载

  1. Click the Download button.
  2. Select the appropriate executable file. 
  3. Choose Run.

如何安装

  • Run the downloaded installer.
  • If you see a Windows Security prompt, check the box Always trust software from "Agilent Technologies, Incorporated", then click the Install button to install the driver.

颁发许可证

  • 不要求具有许可证

支持文档

2011-03-07 1.0.3 M9018A Driver Version 1.0.3 for 18 Slot PXIe Chassis

如何下载

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

如何安装

  • Run the downloaded installer.
  • If you see a Windows Security prompt, check the box Always trust software from "Agilent Technologies, Incorporated", then click the Install button to install the driver.
     

颁发许可证

  • 不要求具有许可证

支持文档