这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家联系

M9018A 18 插槽 PXIe 机箱驱动程序

For a complete list of all instrument drivers from Keysight, please visit www.keysight.com/find/drivers

This driver download installs the IVI-C, IVI-COM, LabVIEW, and MATLAB driver components, as well as the soft front panel and kernel device driver.

Keysight modular drivers also require that Keysight IO Libraries Suite 16.0 or greater be installed. To get the latest release of the IO Libraries Suite, go to www.keysight.com/find/iosuite

Current Version Details
Version 1.2.3
Models Supported M9018A
IO Libraries Required Version 16.2 or greater
Driver Types and Version IVI-C (32/64-bit) 1.2.1.3
IVI-COM (32/64-bit) 1.2.1.3
LabVIEW (32/64-bit) 1.0.5
MATLAB (32-bit) 1.2.1.3
Soft Front Panel Version 1.2.1.3
IVI Classes Supported IviDriver 1.0
Minimum IVI Shared Components Version 2.1.1 

Changes in release 1.6.493.1:

  • Added support for two new Gen3 PXIe Chassis: the 10 slot M9010A and the 18 slot M9019A.

With the addition of these two new PXIe Chassis to the Chassis Family, four chassis are now supported.

  • Added the Keysight Technologies Trigger Manager driver (KtMTrig) to provide an enhanced API (IVI.NET and IVI-C) for making reservations and setting trigger routes on the PXIe Chassis backplane.

With the addition of the Trigger Manger driver, this installer now provides the 3 drivers listed below.

  • Fixed various defects to improve the reliability of PCIe device boot time enumeration.
  • Fixed a defect so the Soft Front Panel can run if the OS language format is set to a value other than English.
  • Changed the default minimum fan speed for the M9010A from 1200 RPM to 900 RPM.
  • Added additional example programs to demonstrate control of Front Panel Trigger Ports and how to use the Trigger Manager.
  • Added a feature to flash LEDs on the chassis front panel for identifying M9010A, M9018B, and M9019A.
  • Enhanced the Soft Front Panel to make it easier to use and included:
  • Display of PCIe link speed and number of lanes for M9010A and M9019A.
  • Display of alarm notification on tab label.

This installer contains 3 drivers:

KtMPxiChassis Driver

  • PXIe Chassis Family driver
  • IVI.NET and IVI-C API
  • See introduction file for additional information

KtMTrig driver

  • Trigger Manager
  • IVI.NET and IVI-C API
  • See introduction file for additional information

AgM9018 Driver

  • Legacy M9018A driver to support applications written for version 1.5.80.1 of AgM9018 driver
  • IVI-C and IVI-COM API
  • See introduction file for additional information
发布日期 版本 版本说明
2017-04-19 1.6.493.1 See description above.

如何下载

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

如何安装

  • Run the downloaded installer.
     

颁发许可证

  • 不要求具有许可证

支持文档

下载

安装于:

PC

操作系统

  • Windows 7
  • WES 7
  • Windows 8.1
  • Windows 10

前提条件

支持的仪器

  • M9010A, M9018A, M9018B, M9019A

相关链接