Keysight recommends using the most current version, which includes the most up-to-date bug fixes and security patches available.
Release Date Version Version Description
2010-04-10 5.0.4 Fixed a ~ 15 μs delay when triggering the start of an ARB waveform.
Release Date Version
2010-04-10 5.0.4
Version Description
Fixed a ~ 15 μs delay when triggering the start of an ARB waveform.

How to Download

  1. Click the Download button
  2. Save the file to your PC

How to Install

  1. Copy the file to a USB thumb drive.
  2. Insert the thumb drive into the V2920A.
  3. Press: Menu, Utilities, Upgrade Firmware, Look In, USB. Select the file and press load.
  4. Wait until the instrument has rebooted.
  5. Press: Menu, Global Settings, Advanced, More. Check the box to turn On the reprogramming of the DSP firmware.
  6. Power cycle the instrument
    IMPORTANT: Do not remove the USB drive or stop the procedure until the instrument has completely rebooted.

Licensing

  • Does Not Require a License

Installs on: Instrument

Prerequisites

  • See Installation Guide

Supported Instruments

  • V2920A
No previous versions available
SHOW MORE