这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家联系

34980A 多功能开关/测量主机和模块 IVI 仪器驱动程序

For a complete list of all IVI drivers from Keysight, please visit IVI-COM and IVI-C Drivers

Keysight IVI drivers also require the Keysight IO Libraries Suite to be installed. To get the latest release of the IO Libraries Suite, go to www.keysight.com/find/iosuite
 

Current Version Details
Version 1.4.2.0
Models Supported 34980A and modules 34921A, 34922A, 34923A, 34924A, 34925A, 34931A, 34932A, 34933A, 34934A, 34937A, 34938A, 34939A, 34941A, 34942A, 34945A, 34946A, 34947A, 34950A, 34951A, 34952A, 34959A
Driver Type IVI-COM and IVI-C
IVI Classes Supported IviDmm 3.0 IVI-COM
IviDriver 1.0 IVI-C
IviDriver 1.0 IVI-COM
IviSwtch 3.0 IVI-C
IviSwtch 3.0 IVI-COM
IVI-C Prefix Ag34980a
ag34945A
ag34951a
ag34952a
ag34959A
IVI-COM ProgID Agilent34980A.Agilent34980A
Agilent34945A.Agilent34945A
Agilent34950A.Agilent34950A
Agilent34952A.Agilent34952A
Agilent34959A.Agilent34959A
.NET Namespace  
Minimum IVI Shared Components Version  
Driver Download See links below.
Readme Download See links below.
Help File Download (.chm)  

Special Note

The standard driver and the NI Switch Executive version have been combined into a single driver starting with revision 1.4.2.0 of the driver.
 

发布日期 版本 版本说明
2015-11-20 1.5.5.0 Fixed defects with 34934A matrix configuration

Driver type: IVI-C (32-bit/64-bit), IVI-COM (32-bit/64-bit), MATLAB (32-bit only), LabVIEW (32-bit/64-bit)

IVI class support: IviDriver 1.0, IviDmm 4.1 (IVI-COM only), IviSwtch 4.0 - the following modules are not supported by the IviSwtch API: 34945A, 34950A, 34951A, 34952A, 34959A

如何下载

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.
     

如何安装

  • Run the downloaded installer.

颁发许可证

  • 不要求具有许可证

支持文档

下载

安装于:

PC

操作系统

  • Windows 7
  • Windows Vista
  • Windows XP

前提条件

支持的仪器

  • Frame: 34980A Modules: 34921A, 34922A, 32923A, 34924A, 34925A, 34931A, 34932A, 34933A, 34934A, 34937A, 34938A, 34939A, 34941A, 34942A, 34945A, 34946A, 34947A, 34950A, 34951A, 34952A, 34959A

相关链接

2013-06-12 1.5.3.0 Defect fixes, added 64-bit IVI driver, added MATLAB wrapper, changed the IviSwtch behavior of Form C (General Purpose) switches.

如何下载

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

如何安装

  • Run the downloaded installer.

颁发许可证

  • 不要求具有许可证

支持文档

下载

安装于:

PC

操作系统

  • Windows 7
  • Windows Vista
  • Windows XP

前提条件

支持的仪器

  • Frame 34980A Module 34921A 34922A 34923A 34924A 34925A 34931A 34932A 34933A 34934A 34937A 34938A 34939A 34941A 34942A 34945A 34946A 34947A 34950A 34951A 34952A 34959A

相关链接

2009-01-09 1.4.2.0 IVI-COM, IVI-C Version 1.4.2.0 for 34980A

如何下载

  • Click the Download button. Select the appropriate executable file. Choose Run.

如何安装

  • See Documentation

颁发许可证

  • 不要求具有许可证

支持文档

下载

安装于:

PC

操作系统

  • Windows 7
  • Windows Vista
  • Windows XP

前提条件

支持的仪器

  • Frame 34980A Module 34921A 34922A 34923A 34924A 34925A 34931A 34932A 34933A 34934A 34937A 34938A 34939A 34941A 34942A 34945A 34946A 34947A 34950A 34951A 34952A 34959A

相关链接

2007-07-16 1.3.10.0 IVI-COM, IVI-C Version 1.3.10.0 for 34980A

如何下载

  • Click the Download button. Select the appropriate executable file. Choose Run.

如何安装

  • See Documentation

颁发许可证

  • 不要求具有许可证

支持文档

下载

安装于:

PC

操作系统

  • Windows 7
  • Windows Vista
  • Windows XP

前提条件

支持的仪器

  • Frame 34980A Module 34921A 34922A 34923A 34924A 34925A 34931A 34932A 34933A 34937A 34938A 34941A 34942A 34945A 34946A 34947A 34950A 34951A 34952A 34959A

相关链接

2006-06-01 1.3.7.0 IVI-COM, IVI-C Version 1.3.7.0 for 34980A
2005-07-01 1.3.1.0 IVI-COM, IVI-C Version 1.3.1.0 for 34980A