Installable Instrument:
This firmware is installable into the following instrument.

  • E5270A
  • E5272A
  • E5273A

Firmware Revision:
A.01.07

Resolved Defects:
The following feature is available.

  • I measurement calibration limit was changed to relax restriction according with hardware specification

Update Instruction:
See the update appl.txt file included in the zipped file.

Keysight recommends using the most current version, which includes the most up-to-date bug fixes and security patches available.
Release Date Version Version Description
2004-11-15 A.01.07 E5270A Series Firmware Rev.A.01.07
Release Date Version
2004-11-15 A.01.07
Version Description
E5270A Series Firmware Rev.A.01.07

How to Download

  • See the update appl.txt file included in the zipped file.

How to Install

  • See the update appl.txt file included in the zipped file.

Licensing

  • Does Not Require a License

Installs on: Instrument

Prerequisites

  • See the update appl.txt file included in the zipped file.

Supported Instruments

  • E5270A, E5272A, E5273A
No previous versions available
SHOW MORE