Click on the url and unzip the zip file contents onto a local directory. This zip file contains the executable file and help file for installing the Utility in order to upgrade the U-Series USB Average Sensors.

If you are unable to view help files downloaded from the Keysight website:

In September 2005, Microsoft® released a security patch for Windows® operating systems that protects PCs from the threat of malicious code that could reside in compiled HTML help files (*.chm files). When a *.chm file is downloaded to a PC that has the patch installed, the file opens with one of the following error messages displayed:

  • Action Canceled
  • The page cannot be displayed

Workaround: After downloading the file to your PC, open it from the location it was saved and a security warning appears. To view the help system, clear the checkmark from the "Always ask before opening this file" check box. The help system can now be viewed from the PC. Alternatively, right-click the file you want to open, click Properties and then click Unblock.

Note: No workaround exists for viewing *.chm files remotely. You must first download the file to your PC and then use the workaround described above.

Microsoft is a U.S. registered trademark of Microsoft Corporation.
Windows and MS Windows are U.S. registered trademarks of Microsoft Corporation.

Keysight recommends using the most current version, which includes the most up-to-date bug fixes and security patches available.
Release Date Version Version Description
2013-01-21 R01.07.00 The U-Series USB Average Sensor Upgrade Utility.
Release Date Version
2013-01-21 R01.07.00
Version Description
The U-Series USB Average Sensor Upgrade Utility.

How to Download

  • Click on the url and unzip the zip file contents onto a local directory. This zip file contains the executable file and help file for installing the Utility in order to upgrade the U-Series USB Average Power Sensors.

Licensing

  • Does Not Require a License

Installs on: PC

Operating System

  • Windows 8
  • Windows 7
  • Windows Vista
  • Windows XP SP3
  • Windows XP SP2

Prerequisites

  • Windows® XP Professional (Service Pack 2 or higher) - Agilent IO Libraries 16.0 or higher

  • Windows Vista Business - Agilent IO Libraries 16.0 or higher

  • Window 7 - Agilent IO Libraries 16.0 or higher

  • Window 8 - Agilent IO Libraries 16.3 or higher

Supported Instruments

  • U2000A,U2001A,U2002A,U2004A,U2000B,U2000HU2001B,U2001H,U2002H,U8485A,U8481A
No previous versions available
SHOW MORE