Here’s the page we think you wanted. See search results instead:

 

Sprechen Sie mit einem Experten

4352B Signal Analyzer Firmware Update

Firmware Installation Procedure:

1. Click on the "4352B Signal Analyzer Firmware Revision X.XX" listed below the page. Copy the file(.src) to a floppy disk. For Firmware version 2.11, rename the file name from "4352update.src" to "Update.src".

2. While pressing [Preset] key of the instrument, turn the instrument power on.

3. Insert the floppy disk into the disk drive.

4. Press 'PREVIEW DISK' softkey. The update disk revision will be displayed.

5. Confirm the displayed "Update Disk Revision" and press Return.

6. Press 'SYSTEM UPDATE' softkey, then 'CONTINUE' to install the firmware from the floppy disk to the instrument. It will take about a few minutes.

7. After "Update Complete" is displayed, press 'REBOOT' softkey to reboot the instrument.

8. Press [System] key, then 'FIRMWARE REVISION' softkey to confirm the current firmware revision. If "POWER ON TEST FAILED" isn't displayed on the LCD and the new firmware revison is correctly displayed, the firmware installation is successfully completed.

Release Date Version Version Description
2000-12-01 2.10 4352B Signal Analyzer Firmware Update Rev 2.10

How to Download

  • Click the download button and save the file to a temporary directory on your PC (or instrument).

How to Install

  • See Above

Licensing

  • Does Not Require a License
Download

Installs on:

Instrument

Prerequisites

  • No specific prerequisites

Supported Instruments

  • 4352B