Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

N4010A Instrument Firmware

N4010A Instrument Firmware
Revision A.05.06.02 - October 18th 2012
Maintenance Release: Customers using either Bluetooth® or Wireless LAN Options are advised to upgrade to this release. Refer to the revision history note for further details of this release.

Instrument Firmware versions prior to A.05.03.12 must be used with a specific revision of the WLAN Test Suite. The table below shows the correlation between Instrument Firmware and WLAN Test Suite revisions.
 

This restriction was relaxed at Instrument Firmware version A.05.03.12 and WLAN Test Suite version 5.5.2:

Instrument Firmware revision A.05.03.12 can be used with WLAN Test Suite revision 5.5.2 or later.

WLAN Test Suite revision 5.5.2 can be used with Instrument Firmware revision A.05.03.12 or later.
When a new version of the WLAN Test Suite is available, the table below will indicate which revision of Instrument Firmware was current at that time.
Note that WLAN Test Suite releases from 5.5.2 onwards do not have duplicate entries in the table, as correlation is no longer necessary.

Please note that in some instances it is possible to downgrade the Instrument Firmware to an older revision without impacting the operational stability or measurement integrity of the unit, but this is not always the case. There are various factors that must be taken into account before attempting a downgrade.
 

For further details, please refer to Service Note N4010A-02C
 

N4010A Instrument Firmware N4010A WLAN Test Suite
Revision A.05.05.01 (6.55 MB) -
Revision A.05.05.00 (6.55MB) -
Revision A.05.04.01 (6.53MB) -
Revision A.05.03.16 (5.96 MB) -
Revision A.05.03.14 (5.95 MB) -
Revision A.05.03.13 (5.96 MB) Revision 6.51 (116 MB
Revision A.05.03.13 (5.96 MB) Revision 6.38 (120 MB)
Revision A.05.03.12 (6.1 MB) Revision 5.5.2 (121 MB)
Revision A.05.03.10 (6.1 MB) Revision 5.4.5 (121 MB)
Revision A.05.03.05 (5.9 MB) Revision 5.4.5 (121 MB)
Revision A.05.03.04 (5.9 MB) Revision 5.4.4 (121 MB)
Revision A.05.02.03 (5.9 MB) Revision 5.4.1 (121 MB)
Revision A.05.02.03 (5.9 MB) Revision 5.3.6 (121 MB)
Revision A.05.01.01 (5.9 MB) Revision 5.1.9 (124 MB)
Revision A.05.01.00 (5.9 MB) Revision 5.1.6 (129 MB)
Revision A.04.05.03 (5.78 MB) Not applicable (Bluetooth® specific firmware)
Revision A.04.05.02 (5.78 MB) Not applicable (Bluetooth® specific firmware)
Revision A.04.04.03 (5.77 MB) Not applicable (Bluetooth® specific firmware)
Revision A.04.03.04 (5.76 MB) Revision 4.0.2 (118 MB)
Revision A.04.02.01 (5.72 MB) Revision 3.1.6a (115 MB)
Revision A.04.01.02 (4.51 MB) Revision 3.1.6a (115 MB)
Revision A.03.01.02 (3.71 MB) Revision 3.1.3a (116 MB)
Revision A.03.01.01 (3.71 MB) Revision 3.0.5 (116 MB)
Revision A.02.00.25 (3.21 MB) Revision 2.0.1 (not available to download)
Revision A.02.00.19 (3.19 MB) Revision 2.0.1 (not available to download)
Revision A.02.00.12 (2.9 MB) Revision 2.0.1 (not available to download)
Revision A.02.00.11 (2.91 MB) Revision 2.0.1 (not available to download)
Revision A.01.17.02 (2.74 MB) Revision 1.0.0.5 (not available to download)
Revision A.01.16.05 (2.7 MB) Revision 1.0.0.5 (not available to download)
Revision A.01.16.04 (2.69 MB) Revision 1.0.0.5 (not available to download)
Revision A.01.15.05 (2.87 MB) Revision 1.0.0.5 (not available to download)
Revision A.01.14.12 (2.72 MB) Revision 1.0.0.5 (not available to download)
Revision A.01.14.11 (2.72 MB) Not available
Revision A.01.14.02 (2.89 MB) Not available
Revision A.01.12 (2.89 MB) Not available
Revision A.01.07 (2.89 MB) Not available
Revision A.01.02 (2.89 MB) Not available

Note: Always install latest version Firmware Upgrade Utility.
 

Release Date Version Version Description
2012-10-18 A.05.06.02 Added support for a new version of the RF Link Subsystem Assembly (“LSS”) board, added an error-checking process at Firmware Upgrade Utility, and more.

How to Download

  • Click on the Download button
  • Select Run
  • Files will be extracted to your hard drive
  • Installation manager will start automatically

How to Install

Licensing

  • Requires a License

Supporting Documentation

Download

Installs on:

Instrument

Prerequisites

  • Information Not Available

Supported Instruments

  • N4010A