Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

IO Libraries Suite Downloads

To find out more about the IO Libraries Suite, visit www.keysight.com/find/iosuite

IO Libraries Suite 2017 includes the following features:

  • Fixed several stability issues that could cause Connection Expert to crash.
  • Fixed an issue where LAN connections would open twice as many sockets as needed.
  • Fixed an issue where aliases didn’t work on all PXI addresses.
  • Fixed an issue where PXI configuration.ini was reset to defaults during installation.
  • Added the ability to set the Method to “User Selected” for the PXI Resource Manager.
  • See readme for complete list of defect fixes
Release Date Version Version Description
2017-06-14 2017 Update 1 See description above. Build 18.0.22209.2

How to Download

  • Click the download link and save the installer.

How to Install

  • Run the downloaded installer.

Licensing

  • Does Not Require a License

Supporting Documentation

Download

Installs on:

PC

Operating System

  • Windows 10
  • Windows 8.1
  • Windows 7 SP1
  • Windows Server 2012 (64-bit only)
  • Windows Server 2008 R2 SP1 (64-bit only)

Prerequisites

  • No specific prerequisites

Supported Instruments

  • All instruments.

Related Links