이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

86100C Infiniium DCA-J Firmware Upgrade

Firmware version A.10.02-A.10.8x is required to connect the 86100C to N1010A FlexDCA Remote Access software running on an external PC.  A.10.83 is recommended for all customers.

NOTE: the 86100C hardware and firmware will not support Microsoft Windows 7.

릴리스 날짜 버젼 버전 설명
2014-05-21 A.10.83 FW A.10.83 offers improved performance when measuring Avg Optical Power.

다운로드 방법

  • Copy the firmware uprade file to a USB flash drive or LAN folder that will be available to the 86100D.

설치 방법

  • On the 86100C, click Exit on the file menu and exit the 86100C application.

    Copy the upgrade file to the user drive (D:) . For best results with large USB file transfers use the rear panel USB ports on the 86100C mainframe.

    Run the installation package, following all instructions to install your new firmware version.

라이센스

  • 라이센스 필요 없음
다운로드

설치 위치:

Instrument

운영 체제

  • Windows XP SP3

사전 조건

  • 86100C DCA-J Mainframe
  • NOTE: The 86100C hardware and firmware will not support Microsoft Windows 7.

지원되는 계측기

  • 86100C