Here’s the page we think you wanted. See search results instead:

 

Parla con un Esperto

N9010A EXA Signal Analyzer Instrument Software

PLEASE NOTE:

  • Instruments running the Windows 7 operating system - See Current Version tab below
  • Instruments running the Windows XP operating sytsem - See Previous Versions tab below

To determine the operating system installed refer to the certificate of authenticity (COA) on the rear panel of the instrument.

Release Date Version Version Description
2017-03-22 A.19.05 Downloadable installation file of the latest software version for instruments running the Windows 7 operating system.

How to Download

  • If your analyzer is connected to the network, download the software update package directly onto the analyzer and run the file.
  • Otherwise, download the package onto your PC and transfer the file to the anlayzer using a USB storage device.
  • Note: Do not run the instrument software executable file on your personal computer. It must run on the anlayzer that is being updated.

How to Install

Licensing

Supporting Documentation