Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

PXIe Chassis Family Drivers

For a complete list of all instrument drivers from Keysight, please visit www.keysight.com/find/drivers

Changes in release 1.6.493.1:

  • Added support for two new Gen3 PXIe Chassis: the 10 slot M9010A and the 18 slot M9019A.

With the addition of these two new PXIe Chassis to the Chassis Family, four chassis are now supported.

  • Added the Keysight Technologies Trigger Manager driver (KtMTrig) to provide an enhanced API (IVI.NET and IVI-C) for making reservations and setting trigger routes on the PXIe Chassis backplane.

With the addition of the Trigger Manger driver, this installer now provides the 3 drivers listed below.

  • Fixed various defects to improve the reliability of PCIe device boot time enumeration.
  • Fixed a defect so the Soft Front Panel can run if the OS language format is set to a value other than English.
  • Changed the default minimum fan speed for the M9010A from 1200 RPM to 900 RPM.
  • Added additional example programs to demonstrate control of Front Panel Trigger Ports and how to use the Trigger Manager.
  • Added a feature to flash LEDs on the chassis front panel for identifying M9010A, M9018B, and M9019A.
  • Enhanced the Soft Front Panel to make it easier to use and included:
  • Display of PCIe link speed and number of lanes for M9010A and M9019A.
  • Display of alarm notification on tab label.

This installer contains 3 drivers:

KtMPxiChassis Driver

  • PXIe Chassis Family driver
  • IVI.NET and IVI-C API
  • See introduction file for additional information

KtMTrig driver

  • Trigger Manager
  • IVI.NET and IVI-C API
  • See introduction file for additional information

AgM9018 Driver

  • Legacy M9018A driver to support applications written for version 1.5.80.1 of AgM9018 driver
  • IVI-C and IVI-COM API
  • See introduction file for additional information
Release Date Version Version Description
2017-04-19 1.6.493.1 See description above.

How to Download

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

How to Install

  • Run the downloaded installer.
     

Licensing

  • Does Not Require a License

Supporting Documentation

Download

Installs on:

PC

Operating System

  • Windows 7
  • WES 7
  • Windows 8.1
  • Windows 10

Prerequisites

Supported Instruments

  • M9010A, M9018A, M9018B, M9019A

Related Links