Here’s the page we think you wanted. See search results instead:


Sprechen Sie mit einem Experten

M9185A PXI 8/16-Channel Isolated D/A Converter Instrument Drivers

This driver download installs the IVI-C, IVI-COM, LabVIEW, and MATLAB driver components, as well as the soft front panel and kernel device driver.

Current Version Details
Models Supported M9185A
IO Libraries Required Version 16.0 or greater
Driver Types and Version

IVI-C (32/64-bit)
IVI-COM (32/64-bit)
LabVIEW (32/64-bit) 1.1.3
MATLAB (32 bit)

Soft Front Panel Version 1.0.0
IVI Classes Supported

IviDriver 1.0

Release Date Version Version Description
2012-11-07 Fixed bug where GetAvailableChannels always return -23728 for parameters "ChannelGroup1" and "ChannelGroup2"

How to Download

  1. Click the Download button.
  2. Select the appropriate executable file.
  3. Choose Run.

How to Install

  • Run the downloaded installer.


  • Does Not Require a License

Supporting Documentation


Installs on:


Operating System

  • Windows 7
  • Windows Vista
  • Windows XP


Supported Instruments

  • M9185A

Related Links