Use the connection you already know!

LXI Version 1.6 - Secure Network Connection

The LXI Version 1.6 has been released, with updated specifications to address the need for secure network communication with LXI devices. These updates include:

  • LXI Security Extended Function: A new specification that establishes requirements for LXI instruments that provide secure network connections for both command-and-control and for the instrument's web interface.
  • LXI API Extended Function: A new specification that specifies a REST API to configure and query the settings on an instrument that are important for the instrument to work in a secure environment.
  • LXI Device specification: Security updates to require an HTTPS web server and not allow the use of a blank password. Several other minor updates were made to incorporate LXI Version 1.5 clarifications and other changes.
  • LXI HiSLIP Extended Function: Updates to require IVI HiSLIP rev 2 which optionally supports secure connections using TLS and Client/Server authentication. These features are optional in the LXI HiSLIP Extended Function but are required if the instrument supports the LXI Security Extended Function.
  • LXI IPv6 Extended Function: Updates to align with the NIST IPv6 Profile requirements, static and DHCPv6 addressing are now required, added more enable/disable capabilities and LXI Extended Functions supported on IPv4 must also be supported on IPv6.

  • The LXI Consortium has been collaborating with the IVI Foundation for several years to identify and develop standards to secure instrument network communication and access in an Automated Test System (ATS).

    For more details on LXI Version 1.6:

  • Press Release - IVI and LXI Leading the T&M Industry in Security Standardization
  • Article - LXI Version 1.6 Security Updates
  • Article - LXI Reference Design Updates for LXI Version 1.6
  • Article - LXI Version 1.6 Conformance Testing with TSEP Kerberos
  • IVI Foundation Security Updates



  • Use the connection
    you already know




    What's New?
    ------------------------------------------------------------- More news

     







    LXI is the robust system backbone for today and tomorrow.

     

    Search for LXI products

    More than 4026 certified LXI products from 54 vendors in over 338 different product families.LXI Products

    LXI Security Working Group

    Learn how LXI addresses cyber security issues

    LXI Reference Design

    Learn how LXI Reference Design provides Member companies with LXI Core and Extended Functions

    LXI Products

    Specifications

    Next generation T&M platform with powerful built-in features