How do I transfer the screen image on my PSA, ESA, or EMC analyzer to a PC using Keysight VEE?
Frequently Asked Questions (FAQs)
Summary
The example below demonstrates the use of the remote commands for transferring the screen image from the instrument. This can be downloaded and run using Keysight VEE 7.0 or later. If you are not using VEE and you would like to see what instrument remote commands are required to do this, you can view the image file instead for a look at what the program contains.Question
How do I transfer the screen image on my PSA, ESA, or EMC analyzer to a PC using Keysight VEE?
Answer
The example below demonstrates the use of the remote commands for transferring the screen image from the instrument. This can be downloaded and run using Keysight VEE 7.0 or later. If you are not using VEE and you would like to see what instrument remote commands are required to do this, you can view the image file instead for a look at what the program contains.
If you do not currently have a copy of VEE, you can go to the VEE web site to find out more about it as well as download a free 30-day trial version: