Column Control DTX

Satellite Earth Stations: Validation, Maintenance and Repair

Application Notes

A satellite communications system is comprised of two segments, one operating in space and one operating on earth. Figure 1 shows a block diagram of the space and ground segments found in a typical satellite communications system. The space segment includes a diverse set of spacecraft technologies varying in operating frequency, coverage area and function. The satellite orbit is typically related to the application. For example, about half of the orbiting satellites operate in a Geostationary Earth Orbit (GEO) that maintains a fixed position above the earth’s equator. These GEO satellites provide Fixed Satellite Services (FSS) including broadcast television and radio. The location of GEO satellites result in limited coverage to the polar regions. For navigation systems requiring complete global coverage, constellations of satellites operate in a lower altitude, namely in the Medium Earth Orbit (MEO), that move around the earth in 2-24 hour orbits. At even lower altitudes, namely in the Low Earth Orbit (LEO), satellites provide applications which include remote sensing and mobile communications. The International Space Station and the Hubble Space Telescope also operate in LEO.
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
By clicking the button, you are providing Keysight with your personal data. See the Keysight Privacy Statement for information on how we use this data.

Thank you.

A sales representative will contact you soon.

Column Control DTX