The system recovery disk (3.5 inch floppy disk) is furnished with the instrument.
If you do not have it, you can make it using the file below.

Download Instructions

  1. Click on the file name listed below the page. Copy the file(.exe) to a temporary directory (e.g. C:TEMP) on your computer's hard drive.
  2. Navigate to the temporary directory where the files are extracted to. Refer to "Procedure to create a backup disk" for detailed instructions.