Column Control DTX

Preamplifiers and System Noise Figure

Application Notes

Preamplifiers 

A preamplifier is an amplifier used in a way such that it usually precedes another amplifier to prepare an electronic signal for further amplification or processing.

 

It is usually a low noise amplifier with moderate gain. For example, in communications systems, the preamplifier is used to amplify the very small signals received by the antenna and is often located very close to the antenna.

 

Using a preamplifier with low noise, the noise of all the subsequent stages is reduced by the gain of the preamplifier and the noise of the preamplifier is injected directly into the received signal. A preamplifier is required to boost the desired signal power while adding as little noise and distortion as possible so that the retrieval of this signal is possible in the later stages in the system.

 

The following sections will give a description of noise and the effect an amplifier has on the sensitivity and noise figure of a system as well as a method for choosing the correct amplifier to meet your measurement needs.
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
By clicking the button, you are providing Keysight with your personal data. See the Keysight Privacy Statement for information on how we use this data.

Thank you.

A sales representative will contact you soon.

Column Control DTX