Do the InfiniiVision Series oscilloscopes provide the ability to switch off the Auto Scale feature?
You cannot do this on the front panel. However, there are remote interface SCPI commands for the InfiniiVision Series oscilloscopes that enable or disable the front panel Auto Scale function.
The commands are:
- AUToscale DISable (disables Auto Scale)
- AUToscale ENABle (enables Auto Scale)
The enable/disable is kind of a permanent setting until it is reprogrammed, as it flips the bit on the non-volatile memory on the oscilloscope.