Starting Download..
save Save

How do I locate the serial number for my 34980A Mainframe?

Frequently Asked Questions (FAQs)

Summary

2 methods for identifying the serial number for my 34980A Mainframe

Question

How do I locate the serial number for my 34980A Mainframe?

Answer

The serial number for the 34980A is located on the rear of the mainframe, on the left vertical face of the connector-cluster section by the LAN and USB connector (see the image below).

image


The serial number can also be retrieved programmatically from the instrument by sending the IEEE 488.2 common command string "*IDN?" to the instrument, and looking at the third returned value (after manufacturer and model).
 

*IDN?
Agilent Technologies, 34980A, MY44002648, 2.19-1.05-2.07-1.05

In this returned string, "MY44002648" is the serial number; yours will be different.

Was this helpful?


Didn't find what you're looking for?