What Does the "LASER PROTECTION" Message for the 8167 Series and 8168 Series Tunable Laser Source (8167A/B, 8168A/B/C/D/E/F) Indicate?
Operational "How to" Guides
Summary
What does the "LASER PROTECTION" message for the 8167 series and 8168 series tunable laser source (8167A/B, 8168A/B/C/D/E/F) indicate?Description
The "LASER PROTECTION" message indicates that the laser has been switched off to prevent damage to the laser diode. The first step is to re-enable the laser to try and clear the error message. If this does not work, try reducing the optical output power, and then re-enabling. The last step before returning the laser to a Keysight Service Center for repair is to perform an automatic laser realign. You should not use automatic realignment when the laser is stabilizing. To perform a realign use the following keystrokes:
Automatic Realignment:
- Press AUX
- Press Realign to initiate the automatic realignment.
If "LASER PROTECTION" message appears frequently, please return the unit to your local service center for evaluation and repair.