Starting Download..
save Save

Can I have multiple math functions (Null, Min-Max, dB, dBm, Limit) turned on at the same time on the 34405A Digital Multimeter?

No, you cannot have multiple math functions (Null, Min-Max, dB, dBm, Limit) turned on at the same time on the 34405A Digital Multimeter. Only one math operation can be turned-on at a time. Selecting another math operation when one is already on will turn off the first operation and turn on the second operation instead.

Was this helpful?


Didn't find what you're looking for?