Can I call other application tests from within an application test using the EasyEXPERT application test editor?
Yes. The EasyEXPERT application test editor is similar in this regard to an object-oriented programming environment. From within the “Test Contents” tab select the “Application Test” sub-tab. You will see a list of all of the application tests contained in the currently selected library categories. [Note: You must select the categories BEFORE opening the application test editor.] EasyEXPERT 2.0 (revision A.02.00 or later) also supports calling application tests that have been modified and saved into a “My Favorites” setup. From within the “Test Contents” tab select the “My Favorite Setup” sub-tab. You can then select and insert application tests that have been saved into a “My Favorites” list.
Learn more about Keysight EasyEXPERT/Desktop EasyEXPERT Device Characterization Software.