How do I recover my B1500A in case I have a problem? I did not receive a Windows OS recovery CD with my instrument.
There is no windows recovery CD supplied with the instrument. Instead, a portion of the hard disk drive is partitioned with a recovery image that you can use to return the B1500A to its virgin state. However, any current data on the instrument will be lost if you perform this process, so you need to back up your data before performing a recovery. For more information on this process, please refer the EasyEXPERT User’s Guide.