Microsoft Windows Security Updates
The following Microsoft ® Windows ® security updates are compatible with the B1500A.
- msxml4-KB954430-enu.exe
- NDP1.1sp1-KB929729-X86.exe
- WindowsXP-KB955069-x86-ENU.exe
- WindowsXP-KB956802-x86-ENU.exe
- WindowsXP-KB958215-x86-ENU.exe
- WindowsXP-KB958687-x86-ENU.exe
- WindowsXP-KB958690-x86-ENU.exe
- WindowsXP-KB960714-x86-ENU.exe
- WindowsXP-KB960803-x86-ENU.exe
- WindowsXP-KB961373-x86-ENU.exe
- WindowsXP-KB963027-x86-ENU.exe
Download patches and security information from the Microsoft website. Search by the security update number. http://www.microsoft.com/athome/security/default.mspx
The following security updates are pre-installed.
- NDP1.1sp1-KB928366-X86.exe
- WindowsMedia9-KB917734-x86-ENU.exe
- WindowsMedia9-KB954156-x86-ENU.exe
- WindowsXP-KB904706-x86-ENU.exe
- WindowsXP-KB908519-x86-ENU.exe
- WindowsXP-KB908531-v2-x86-ENU.exe
- WindowsXP-KB914388-x86-ENU.exe
- WindowsXP-KB914389-x86-ENU.exe
- WindowsXP-KB917159-x86-ENU.exe
- WindowsXP-KB918439-x86-ENU.exe
- WindowsXP-KB920213-x86-ENU.exe
- WindowsXP-KB920214-x86-ENU.exe
- WindowsXP-KB920670-x86-ENU.exe
- WindowsXP-KB920683-x86-ENU.exe
- WindowsXP-KB923191-x86-ENU.exe
- WindowsXP-KB923414-x86-ENU.exe
- WindowsXP-KB923689-v2-x86-ENU.exe
- WindowsXP-KB923694-x86-ENU.exe
- WindowsXP-KB923789-x86-ENU.exe
- WindowsXP-KB924270-x86-ENU.exe
- WindowsXP-KB925902-x86-ENU.exe
- WindowsXP-KB927779-x86-ENU.exe
- WindowsXP-KB928843-x86-ENU.exe
- WindowsXP-KB930178-x86-ENU.exe
- WindowsXP-KB931261-x86-ENU.exe
- WindowsXP-KB932168-x86-ENU.exe
- WindowsXP-KB935839-x86-ENU.exe
- WindowsXP-KB935840-x86-ENU.exe
- WindowsXP-KB938127-x86-ENU.exe
- WindowsXP-KB938464-x86-ENU.exe
- WindowsXP-KB941644-x86-ENU.exe
- WindowsXP-KB943055-x86-ENU.exe
- WindowsXP-KB943460-x86-ENU.exe
- WindowsXP-KB944338-v2-x86-ENU.exe
- WindowsXP-KB948590-x86-ENU.exe
- WindowsXP-KB950749-x86-ENU.exe
- WindowsXP-KB950760-x86-ENU.exe
- WindowsXP-KB951066-x86-ENU.exe
- WindowsXP-KB951376-v2-x86-ENU.exe
- WindowsXP-KB951698-x86-ENU.exe
- WindowsXP-KB952954-x86-ENU.exe
- WindowsXP-KB956390-x86-ENU.exe
- WindowsXP-KB958644-x86-ENU.exe
NOTE: The tested B1500A software configuration is as follows. Please confirm the revision of your B1500A.
- O/S: Windows XP Pro SP2
- EasyEXPERT: A.03.20.2008.1030
- Firmware: A.03.20.2008.1028, P.A.03.20.2009.0106
Precautionary Statement
The Keysight B1500A Semiconductor Device Analyzer operates in the Microsoft Windows XP Professional environment. The Keysight B1500A requires the Keysight EasyEXPERT software, a specially-designed Windows XP application program.
About guarantee and support for the Keysight B1500A
Keysight Technologies guarantees and supports the performance of the Keysight B1500A for the same condition as the preload condition when shipped from the factory.
About updating the Keysight EasyEXPERT and the Windows Update
Keysight Technologies confirms the operation of the Keysight EasyEXPERT patch programs and important Windows security patches, and provides recommended update information. Visit the Keysight B1500A support site, download the patches, and perform the software update.
About Windows XP application programs and peripherals (including driver)
Using commercial products on the Keysight B1500A is your responsibility. Keysight Technologies cannot provide compatibility information for commercial products. If problems arise, perform the Keysight B1500A system recovery.
About servicing
- Bench repair service is available at your nearest Keysight Technologies service center. Be aware that the B1500A configuration might be updated to the latest one without notice because of support issues.
- The internal hard disk drive (HDD) might be initialized during servicing. If peripherals are connected, they will be removed.
- When the Keysight B1500A is returned, the internal HDD might be initialized. Peripherals will be returned separately.
Other notes
- Back up the internal HDD to prevent loss of data by accident or failure.
- Protect the Keysight B1500A from computer viruses.
- If you connect the Keysight B1500A to the network, take care to protect it from computer virus.
Microsoft and Windows are U.S. registered trademark of Microsoft Corporation.