Column Control DTX

Replace 34401A 6.5 Digit Multimeter with New 34410A/11A DMM

Application Notes

Introduction

The Keysight Technologies, Inc. 34410A and 34411A represent the latest generation of 61/2-digit multimeters from Keysight Technologies. These new DMMs build upon the phenomenal success of the industrystandard Keysight 34401A and have significantly enhanced functionality for bench and system users. Expanded ranges and accuracy, significantly faster measurement and system speeds along with added functions such as capacitance, temperature, and peak detection capability provide the ability to measure more complex signals.

This application note explains how to migrate from the Keysight 34401A to the new Keysight 34410A and 34411A digital multimeters. We will answer questions such as: “Will these new DMMs drop into my application and run? Is there some compatibility switch? What functionality is the same? What is different? How are these two new DMMs superior in performance to the 34401A?” Topics will include feature comparisons, 34401A emulation mode, measurement speed comparisons, programming/ interfacing differences, and electrical/mechanical differences. For a closer look at how to get the most performance out of the new Keysight DMMs, please refer to Application Note 5989-4039EN, Keysight 34410A/ 34411A 61/2-Digit High-Performance Multimeters.
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
By clicking the button, you are providing Keysight with your personal data. See the Keysight Privacy Statement for information on how we use this data.

Thank you.

A sales representative will contact you soon.

Column Control DTX