IO Libraries Suite: Is there any other software that needs to be installed when I am using an application that utilizes NI-488.2 and Keysight IO Lib...
IO Libraries Revisions: Suite 14.2 and greater
You need to explicitly enable Keysight 488. To do this, click Tools > Keysight 488..., then select the check box labeled Enable Keysight GPIB cards for 488 programs.
Note: Although Keysight 488 does not conflict with NI-488.2 and both libraries can be used simultaneously, some versions of NI-488.2 may report the error message "Missing or Damaged GPIB-32.DLL" when you attempt to use National Instruments Measurement & Automation Explorer (NI MAX) to change the properties of an NI GPIB interface. If this occurs, upgrade to NI-488.2 version 2.5 (or later). You can get the latest NI software at www.ni.com
For more information, see the Keysight Connectivity Guide topic "Using Keysight 488 in Multi-Vendor Systems."
Last Updated: 01September, 2009