Column Control DTX

Parasitic Capacitance and Inductance Using TDR

White Papers

Time Domain Reflectometry (TDR) is commonly used as a convenient method to determine the characteristic impedance of a transmission line, or to quantify reflections caused by discontinuities along or at the termination of a transmission line. TDR can also be used to measure quantities such as the input capacitance of a voltage probe, the inductance of a jumper wire, the end to end capacitance of a resistor, or the effective loading of a PCI card. Element values can be calculated directly from the integral of the reflected or transmitted waveform.

×

Please have a salesperson contact me.

*Indicates required field

Preferred method of communication? *Required Field
Preferred method of communication? Change email?
Preferred method of communication?

By clicking the button, you are providing Keysight with your personal data. See the Keysight Privacy Statement for information on how we use this data.

Thank you.

A sales representative will contact you soon.

Column Control DTX