Technical Overviews
High performance mm-wave source modules extend the frequency coverage of the PSG to 500 GHz.
The Keysight Technologies, Inc. PSG signal generators (PSG) provide excellent signal power, resolution, stability, and analog modulation performance for coaxial applications to 67 GHz. Now, when paired with new, high power mm-wave source modules from OML, Inc., much of the PSG’s capability can be extended up to 500 GHz to meet the requirements of emerging mm-wave applications.
Characteristics of the millimeter-wave spectrum
While it is generally recognized that mm-wave frequencies are between 30 GHz and 300 GHz, factors such as broadband solid state microwave electronics, relatively low atmospheric absorption of signals < 50 GHz, the need for high communication bandwidths, and advances in coax transmission capabilities have allowed the microwave band to virtually encompass the 30 GHz to 50 GHz frequency applications.
The mm-wave spectrum beyond 50 GHz offers many advantages to certain applications. Millimeter-wave wavelengths are small (< 10 mm) which means mm components are smaller than microwave components. This in turn results in smaller, more focused transmit and receive antennas – with apertures that have narrower beam widths and transmissions that suffer less losses in the presence of rain, smoke, fog, and dust.
Atmospheric constituents and gases attenuate millimeter signals at different rates for different frequencies. Overall, there are narrow regions (bands) of high signal absorption and wide regions of low signal absorption that occur over the entire millimeter frequency range. The low absorption bands provide sufficient bandwidth for localized applications such as automotive collision radar or autonomous cruise control (77, 94 GHz), broadband gigabit wireless communications (70 to 86 GHz), non-ionic imaging (110 to 300 GHz), material characterization and chemical sensing (225 to 310 GHz).
Solving your mm-wave signal source needs
Millimeter wave sources are essential instruments for developing almost all millimeter wave systems and for extending the range of microwave systems. The SxxMS-AG series of high power, frequency banded mm-wave source modules from OML, Inc., when driven by Keysight’s high performance PSG, provide synthesized mm-wave test signals for waveguide bands from 50 to 500 GHz. The SxxMS-AG series have RF input power protection allowing all PSG’s with high output power (Option 1EU or 1EA) to drive mm-wave source modules without the need for external RF power amplifiers. In addition, the SxxMS-AG series were designed to derive DC power directly from the PSG (through the source-module-interface connector), and eliminates the need for an external DC power supply.
High accuracy and resolution
Because the SxxMS-AG series modules employ frequency multiplication to generate mm-wave frequencies, the output frequency specifications are directly proportional to the characteristics of the PSG driving the module. The PSG’s frequency resolution is typically in the millihertz range, which allows a mm-wave carrier frequency of 500 GHz to have a frequency resolution of < 1 Hz.
Spectral Purity
The SxxMS-AG series mm-wave source modules offer harmonic, sub-harmonic, and spurious suppression of > 20 dBc, in any band. The high stability and low phase noise performance of the PSG is raised by a factor of 20 log N, where N is the multiplier factor of the specific module. For the eight SxxMS-AG series modules, N varies from 4 (50 to 75 GHz model) to 30 (325 to 500 GHz model) and 20 log N varies from 12 dB (50 to 75 GHz) to 18 dB (90 to 140 GHz) to 30 dB (325 to 500 GHz).
Output Power
The SxxMS-AG series modules offer substantial fixed output power, allowing them to be used as LO's in mixer measurements and provides additional dynamic range for insertion loss/gain measurements. For example, the W-band performance shown in Figure 3 demonstrates a measured output power of +7 dBm with typical output power flatness of ± 1 dB.
The output signal power is fixed and can only be varied through the use of an external fixed attenuator, an external mechanical variable attenuator, or an external electronic variable attenuator.
Excellent FM, PM and Pulse Modulation
FM and/or PM may be applied to the SxxMS-AG series module input signal with the corresponding mm-wave output signal being modulated with an FM/PM deviation that is N times the input deviation (no change in the FM/PM rate) where N is the multiplier factor of the SxxMS-AG module.
The pulse modulation characteristics of the input signal are reproduced faithfully, with the exception of pulse rise and fall times. The non-linear characteristics of the source module will typically produce an output signal pulse with faster rise and fall times. Faster rise and fall times will also yield a small increase in the width of the pulse.
AM and Vector Modulation
The non-linear multiplication characteristics of the SxxMS-AG series do not allow replication of linear AM (sinusoidal amplitude modulation) or vector modulated signals.
Easy connection and operation
The SxxMS-AG has been designed to work directly with the PSG source-module interface (SMI) power supply specifications. Once the SxxMS-AG module is connected to the PSG via the SMI cable and an RF cable (Figure 5), the PSG user interface can be configured to directly display the mm-wave output frequency.
Connect the SxxMS-AG module per Figure 5. Then follow the PSG key steps shown in Figure 6 to select the appropriate mm-wave frequency band for the connected module. Once the OEM source module “ON” selection has been made, the frequency shown on the PSG will be the output frequency of the mm-wave source module. To change the output frequency of the source module, simply enter the desired mm-wave output frequency into the PSG, and the PSG will do the rest. The amplitude value shown on the PSG is the output power of the PSG, and it must be set to +16 dBm for optimum performance of the source module.
×
Please have a salesperson contact me.
*Indicates required field
Thank you.
A sales representative will contact you soon.