How can I recover my E2929B from an interrupted firmware upgrade?
- On the E2929B board set Jumper #3 of S101 to Off
- Power on the E2929B. The Hex display should now show CorJ or CorR.
- Open the file best.ini which is located in the bin directory of your installation path.
- Add the line CoreOpen = TRUE
- Now open the GUI and you should be able to connect to the testcard. The GUI will give you some messages about missing capabilities, but that is ok.
- Next open the Command Line Interface (CLI).
- Enter the command biosload file="../hw/bios_hex.mot". The command should download the latest firmware. It will take approximately 1 minute.
- Finally, return jumper #3 of S101 to On, close the GUI and cycle power on your E2929B.
You should be able to continue with the normal hardware update.